This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Issue with Dual-Core Configuration and GSRAM Validation on F28379D (sysconfig 1.23.0)

Part Number: TMS320F28379D
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

Tool/software:

I’m working with the dual-core example memcfg_ex1_sysconfig located at <root>\ti\C2000Ware_5_04_00_00\driverlib\f2837xd\examples\dual\memcfg. However, I’m encountering a warning: "The memcfg module is needed on CPU1 to assign GSRAM to CPU2."

While I understand that I can suppress this warning to bypass it, I need to use the validation between the cores configuration in my real project.

Setup Overview:

  • Problem: The GS14 RAM is configured on CPU1 to be controlled by CPU2, as shown in my setup, but the warning is triggered on CPU2 instead.

  • Potential Related Issue: This issue may be linked to a post I found on the TI E2E forum: Link to related post

My Environment:

  • CCS Version: 12.8.1.00005

  • C2000Ware Version: 5.4.0.00

  • SysConfig Version: 1.23.0

  • Target Device: F28379D 337ZWT

  • OS: Windows 10

Questions:

  • Is there a workaround to validate the dual-core configuration for my specific use case?

  • Has anyone encountered this issue and found a solution that doesn't involve suppressing the warning?

Any insights or suggestions would be greatly appreciated. 

Thank you!

---

Screenshots:

Configuration of GS14 to be controlled by the CP2.

But the warning is shown in CPU2.