This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P550SJ: CLA

Part Number: TMS320F28P550SJ


Tool/software:

Hi there!
I am working on the new C2000 microcontroller- the P55 series. I am currently migrating from F28379D to F28P55 and I found an interesting thing wrt CLA. While I worked on F28379D, I developed the project over an existing F28379 CLA library examples. In that project, I could find some CLA libraries that are included which is shown in the project explorer image. In the corresponding .cla file, CLAasin() is used like any other function. However, when I open some CLA examples in F28P55 or F28379D device support examples, I cannot find any libraries included in the project and the corresponding .cla files didnt  use simple CLAsin() functions but functions like &CLAasinTable[] were used! Can anyone explain this idea and I cant find all three equivalent library files.

Here are the list of libraries available in the CLA library folder.

As I mentioned about missing libraries, for example, I just borrowed F2837xRevB_c1bootROM_CLADataROMSymbols_fpu32 library from the examples provided in the CLA library examples(not device support CLA example) just to make sure CLAasin() works. 

To conclude I would like to know, to use CLAasin() function on P55 microcontrollers, what libraries shall I use?

Thanks for going through the question.

Regards,

Rajesh.