This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Concerto Control Card Flashing

Other Parts Discussed in Thread: CONTROLSUITE

Hello,

I am trying to program the M3 on the concerto control card with the blinky code example.  I removed the .cmd linked in RAM file and replaced it with F28M35M52C1_m3.cmd.  Are there any other modifications necessary that are required to flash the M3?  I have the board jumper settings all set to the ON Position.  I power cycle the board and I am not able to get blinky to run.  I am starting to check out the dual code example flash.  Let me know if you have documentation that explains this.

-Jason

  • Hi Jason,

    The latest release of controlSUITE should have a blinky_m3 project which contains two (2) build configurations which can be changed through Right Click on Project Name > Active Build Configuration > Flash.  This build configuration should allow you to program the M3 flash blinky code example.  After programming the device, terminate the debug session, turn off power to the controlCARD, set all four switches of SW1 in the DOWN position, and return power to the controlCARD.  LD3 should now be blinking.  Let me know if you are still having issues after following this process.

    The following post has a few links which could be helpful debugging future issues or for more information related to running code from flash on the Concerto device:

    http://e2e.ti.com/support/microcontrollers/tms320c2000_32-bit_real-time_mcus/f/171/p/126824/554976.aspx#554976

    Regards,

    Mark-