This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Errors in Sample Code for F28P65x

Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: LAUNCHXL-F28P65X, C2000WARE

For LaunchXL-F28P65X we want to test the sample programs provided with C2000ware. In this case, the "EtherCAT CPU1 PDI HAL Test CCS" simple test program for the EtherCAT sub-component (complete path in the doc: "C2000 / Embedded Software / C2000 Ware / English / Libraries / Communication / EtherCAT / Examples / F28P65x / EtherCAT CPU1 PDI HAL Test CCS".

This does not run since there are some hard-coded references to the ControlCard evaluatin board.

First, a global define of "_LAUNCHXL_F28P65X" must be made, otherwise the wrong definitions are selected.

Second, all references to e.g. CCARD_LED_1_GPIO must be replaced with DEVICE_GPIO_PIN_LED1.

What is going on here? Does the sample code really run only on control card hardware?

What else do we have to do to run it on LaunchPad hardware?

Does this error apply to all of Texas' sample code for the F28P65x?