Hello,
I want to use SPEED_PR_MACRO(speed1) macro in my motor speed control project. After adding this macro compiler gives an error such that unresolved symbols remain and error encountered during linking. When line 325 in TriggeredADC-Main.c is commented that is SPEED_PR_MACRO is removed error is corrected. What can be the reason?
At the beginning of the .c file that I invoke SPEED_PR_MACRO respective header files which are given below included.
#include "PeripheralHeaderIncludes.h"
#include "DSP2802x_EPwm_defines.h" // useful defines for initialization
#include "IQmathLib.h"
#include <math.h>
#include "PID_REG3.h"
#include "speed_pr.h"
#include "DSP2802X_Gpio.h"
Module usage is also shown below.
SPEED_MEAS_CAP speed1, speed2;
To Instance pre-initialized objects
SPEED_MEAS_CAP speed1 = SPEED_MEAS_CAP_DEFAULTS;
SPEED_MEAS_CAP speed2 = SPEED_MEAS_CAP_DEFAULTS;
Invoking the computation macro
SPEED_PR_MACRO(speed1);
SPEED_PR_MACRO(speed2);
I also attach project file (triggeredADC) to help solving problem.
Best Regards,
Rasit GOKALAN