This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am trying to simulate my code in code composer studio. I am using TMS320F2808.
When I start running my code(in simulator) I am getting message "Trouble running Target CPU: Can't write to data memory 0x801, check memory config".
Every time I press F5 (run) key it shows can't write to data memory.
I have included "sim2808.gel" file in my project. I am having one cmd file which is not reffering to 0x800 location.
Please let me know, if I have specify problem in more detail.
Please help me out.
Regards,
PanShi
Hi,
maybe you're missing this step: after compile your code, in CCS you have to load the program (.out file): "File -> Load program".
Many informations here.
Hi,
Thanks for your immediate reply.
After loading program it is showing following error message. "Can't Run the Indicated Number of Instructions on the Target CPU: Can't write to data memory 0xAEC0, check memory config [-2184] ".
I am going through the link you have mention.
Regards,
panshi
There's a problem with memory mapping, maybe in the .cmd file or in the sim*.cfg or some differences between them.. try to compare the memory definitions of these two files. The sim28xx.cfg is in <CCSpath>\drivers\.
Which is the instruction or portion of your code that gives you this error?
Hi,
I could not see which instruction are at address 0xaec0., but my memory map file shows,
.ebss 1 00008040 00002f00 UNINITIALIZED
00008040 00002e66 BL_InitSettings.obj (.ebss)
0000aea6 00000004 rts2800_ml.lib : _lock.obj (.ebss)
0000aeaa 00000001 : errno.obj (.ebss)
0000aec0 00000080 : exit.obj (.ebss)
In my sim2808.gel file it shows that,
/* Data memory maps */
GEL_MapAdd(0x0,1,0x400,1,1); /* M0 SARAM */
GEL_MapAdd(0x400,1,0x400,1,1); /* M1 SARAM */
GEL_MapAdd(0x800,1,0x800,1,1); /* PF0 */
GEL_MapAdd(0x6000,1,0x1000,1,1); /* PF1 */
GEL_MapAddStr(0x7000,1,0x1000,"R|W|AS2",0); /* PF2 */
GEL_MapAdd(0x8000,1,0x1000,1,1); /* L0 SARAM */
GEL_MapAdd(0x9000,1,0x1000,1,1); /* L1 SARAM */
GEL_MapAdd(0xa000,1,0x2000,1,1); /* H0 SARAM Mirror */
GEL_MapAdd(0x3d7800,1,0x800,1,0); /* OTP */
GEL_MapAdd(0x3e8000,1,0x10000,1,0); /* FLASH */
GEL_MapAdd(0x3f8000,1,0x1000,1,1); /* L0 SARAM Mirror */
GEL_MapAdd(0x3f9000,1,0x1000,1,1); /* L1 SARAM Mirror */
GEL_MapAdd(0x3fa000,1,0x2000,1,1); /* H0 SARAM */
GEL_MapAdd(0x3ff000,1,0x1000,1,0); /* BOOT ROM */
And in my custom cmd file definations are like this,
PAGE 1 : /* Data Memory */
RAMM0 : origin = 0x000000, length = 0x000800 /* on-chip RAM block M0 */
RAML1 : origin = 0x008030, length = 0x03FD0 /* on-chip RAM block L1 */
RAMH0 : origin = 0x3FA000, length = 0x002000 /* on-chip RAM block H0 */
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA PAGE = 0
.stack : > RAMM0 PAGE = 1
.ebss : > RAML1 PAGE = 1
.esysmem : > RAMH0 PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
From this defination I understood that, in sim2808.gel file my H0 SRAM placed at 0xA000 to 0xC000 but in my custom cmd file H0 sram placed at 0x3fa000.
Is this thing causing problem?
I have tried to relocate memory section im my .cmd file to match with sim2808.gel file bit it doesn't work. It is giving compile error such as memory overlap.
Thanks,
Regards,
panshi
Hi,
you have the object "exit" mapped at that location. I think the problem it's the incoherence of your definition with the simulator config (not the .gel file but sim28xx.cfg).
You have the following cmd:
RAMM0 : origin = 0x000000, length = 0x000800 /* on-chip RAM block M0 */
RAML1 : origin = 0x008030, length = 0x03FD0 /* on-chip RAM block L1 */
try to replace that with the following, 'cause RAML1 should go from 0x9000 to 0x9FFF and RAMM0 from 0x0 to 0x3FF while RAMH0 definition is correct:
RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
Raffa
Hi,
I have modify my custom cmd file for
RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */
RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
After doing this I am getting following error message,
>> error: can't allocate .ebss, size 00002f00 (page 1) in RAML1 (avail:
00001000)
>> error: errors in input - ./Debug/ACB0052.out not built
>> Compilation failure
This means that ebss size ( which I have placed in RAML1) is excedding the 4K.
How I can reduce ebss size so that it will fit in to RAML1?
You said " I think the problem it's the incoherence of your definition with the simulator config (not the .gel file but sim28xx.cfg)." but I am not using this file in my project. It is there in C:\CCStudio_v3.1\drivers.
Is it require to modify this file so as to match with my custom.cmd file?
Thanks,
panshi
Hi,
I am still stuck with the same problem.
Please help me out.
Let me know if you need more description of the problem.
Now In custom cmd file I have define HO SARAM memory section as,
RAMH0 : origin = 0x009000, length = 0x003000 /* on-chip RAM block H0 */( I have done so because if I am defineing this memory from 0xa000 to 0xC000 and mapping my ebss to this section then it is giving compiler error i.e. memory overlop.)
From my memory map I can conclude that my ebss section memory requirement is 0x2f00.
" name origin length used attr fill
RAMH0 00009000 00003000 00002f00 RWIX "
When I am starting simulation, and doing go to main action it shows "Can't write to data memory 0xBE80, check memory config [-2184]" message.
If my required memory is 0x9000 to 0x2f00, and in map it is showing that this much meory is allocated then what could be the reason for error?
One more point I have notice in map file,
"
.ebss 1 00009000 00002f00 UNINITIALIZED
00009000 00002e66 BL_InitSettings.obj (.ebss)
0000be66 00000004 rts2800_ml.lib : _lock.obj (.ebss)
0000be6a 00000001 : errno.obj (.ebss)
0000be80 00000080 : exit.obj (.ebss) "
exit is located at 0xbe80 lcoation for which I am getting error.
Regards,
panshi
Hi,
My simulation problem is now solved.
You was right Raffa, there was config difference in sim28xx.cfg file.
Other problem I am facing is that, I am using cycle simulator (since my controller is TMS320F2808) and I have some device configuration (such as PIE) in my code.
Cycle simulator is not supporting peripheral debug and it is giving message "Can't read from data memory 0xCE0" while debugging. What could be the other way I debug my entire code with simulator.
Regards,
panshi
The F28xx cycle simulator does not support peripheral debug as you have seen. The sim28xx.cfg will show you the memory regions the simulator has access to. Since it does not have access to 0xCE0 you are seeing the "Can't read from data memory" message when debugging. You would need hardware like eZdsp to debug peripheral code.
In my case, it was memory configuration (mismatch) issue.
Please look for your .cfg file.
Ensure that you are refering right .cfg file.
In .cfg file ensure that OTP memory and other memory type is properly mapped.
panshi
Thanks Panshi, I found my issue to be similar. The memory map in my *.cmd file did not match that in the simulators *.cfg file (F28xx simulator ). It was a simple fix. I changed the location of my high data memory in the *.cmd file to match that which was in the simulators *.cfg. The simulator is working great now. Cheers Dave
Hi There,
Seems we all have the same problem, however it seems you found the answer. Can I ask someone to post here his *.cmd file and his *.pjt (to see the build options) ?
I cannot manage to have the simulator running. Should be a simple thing but it's not clear to me. I did not change anything in the sim28x.cfg (should I ?), so what should my cmd file looks like ?
Hi There
Maybe there are different reasons possible for this error message. I have the same:
Message: "Error: Can't write to data memory 0x801, check memory config [-2184]"
CCS: Version 3.3.38
Simulator: F2812 Device Simulator
I searched for differences between the memory definitions of "f2812_sim.ccs" and "F2812_EzDSP_RAM_lnk.cmd" but it was consistent.
The instruction where the error appears is "MOV AL,@35" belonging to "while(PieCtrlRegs.PIEIFR1.all != 0x0000 ){}"
Thanks for any inputs.
In a previous post someone reported the error, and a TI employee answered there was a "bug" in the sim file, and that only F28335 will be supported in the future. In CCSv4 only F28335 will be supported.
Sorry to say that but I simply stopped using the simulator and now work only with hardware connected :-(
Hello André. I get it. With HW connected it's better. I just tried to by-pass the time 'til the emulator arrives, by simulating the code. Thanks for your fast answer.
Hi,
I have the same problem of Error: Can't write to data memory 0x800, check memory config [-2184] , when i run my program this error appears. Please i need help in clearing this error. I need help in fixing thisproblem
I am working on Timer0 interrupt ( PIE related) once i run my program this error appears and i tried to debug my program with break points the code jumps to ITRAP0 ( OPCODE 0X0000) and after after this still i continued debugging to check what is status of my timer0 counter value ( in memory window) it continues to decrements and rolls over to zero and then sets TIE bit in TIMER0 control register and if i still continue debugging after some time Stack point register crosses 0X800 value and causing Error message in message window.
I tried all the solutions mentioned in the earlier replies of this post but nothing is working out. I don't have hardware right now to connect, is connecting hardware fixes this problem? Ti Me can you please tell me how did you cleared your problem?.
In my main code i encounter ITRAP0 just one instruction after EINT ( INTM is cleared i.e global interrput bit set). i am attaching my main() function .c file
the file " Example_281xCpuTimer.c" which has function main() and ISR function. i am attaching for reference
// TI File $Revision: /main/3 $ // Checkin $Date: July 2, 2007 11:33:22 $ //########################################################################### // // FILE: Example_281xCpuTimer.c // // TITLE: DSP281x Device Getting Started Program. // // ASSUMPTIONS: // // This program requires the DSP281x V1.00 header files. // As supplied, this project is configured for "boot to H0" operation. // // Other then boot mode configuration, no other hardware configuration // is required. // // DESCRIPTION: // // This example configures CPU Timer0 and increments // a counter each time the timer asserts an interrupt. // // Watch Variables: // CpuTimer0.InterruptCount // //########################################################################### // $TI Release: DSP281x C/C++ Header Files V1.20 $ // $Release Date: July 27, 2009 $ //########################################################################### #include "DSP281x_Device.h" // DSP281x Headerfile Include File #include "DSP281x_Examples.h" // DSP281x Examples Include File // Prototype statements for functions found within this file. interrupt void cpu_timer0_isr(void); void main(void) { int i,x; // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP281x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initalize GPIO: // This example function is found in the DSP281x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP281x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP281x_DefaultIsr.c. // This function is found in DSP281x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.TINT0 = &cpu_timer0_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in DSP281x_InitPeripherals.c // InitPeripherals(); // Not required for this example InitCpuTimers(); // For this example, only initialize the Cpu Timers // Configure CPU-Timer 0 to interrupt every 10 micro second: // 100MHz CPU Freq, ConfigCpuTimer(&CpuTimer0, 100, 10); // PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; StartCpuTimer0(); // Step 5. User specific code, enable interrupts: // Enable CPU INT1 which is connected to CPU-Timer 0: // Enable TINT0 in the PIE: Group 1 interrupt 7 PieCtrlRegs.PIEIFR1.bit.INTx7 = 1; // added by me PieCtrlRegs.PIEIER1.bit.INTx7 = 1; //PieCtrlRegs.PIEACK.all = 0X0001; // added by me IER |= M_INT1; // Enable global Interrupts and higher priority real-time debug events: EINT; // Enable Global interrupt INTM // ERTM; // Enable Global realtime interrupt DBGM x=0; i=1; x=i; // Step 6. IDLE loop. Just sit and loop forever (optional): for(i=0;i<1000;i++) x=i; } interrupt void cpu_timer0_isr(void) { CpuTimer0.InterruptCount++; // Acknowledge this interrupt to receive more interrupts from group 1 PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; asm("IRET"); } //=========================================================================== // No more. //===========================================================================
my linker files are
MEMORY
{
PAGE 0 :
RAMM0 : origin = 0x000000, length = 0x000400
BEGIN : origin = 0x3F8000, length = 0x000002
PRAMH0 : origin = 0x3F8002, length = 0x000FFE
RESET : origin = 0x3FFFC0, length = 0x000002
PAGE 1 :
/* For this example, H0 is split between PAGE 0 and PAGE 1 */
RAMM1 : origin = 0x000400, length = 0x000400
DRAMH0 : origin = 0x3f9000, length = 0x001000
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
ramfuncs : > PRAMH0 PAGE = 0
.text : > PRAMH0, PAGE = 0
.cinit : > PRAMH0, PAGE = 0
.pinit : > PRAMH0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
.ebss : > DRAMH0, PAGE = 1
.econst : > DRAMH0, PAGE = 1
.esysmem : > DRAMH0, PAGE = 1
}
i also referred document on "TMS320f2812_errata" to fix if any stack over flow and tried to change M1 memory and tried to a lower its size but even those fixes did not work.
please help to fix this problem.
Thanks,
Sangeetha