Other Parts Discussed in Thread: TMS320F2810
Hi,
I am wondering if it's possible to use DSP/BIOS on a third party board with a F2810 DSP. I managed to configure a quite simple project with CCS 3.1.30 which compiled without errors and warnings.
It is also running on the hardware, but whenever I click on an object in the DSP/BIOS menu (e.g. CPU Load Graph) I get an error "CBD File Error. The associated CBD file may be missing or corrupted. Use the Configuration Tool to verify that the CBD file does not have any invalid records."
Well, I used a seed file called c28xx.cdb and changed nothing except adding a task. (File->New->DPS/BIOS Configuration...) What can I do to use that features?
Thank you in advance,
Lutz Brandt