Champs,
I have two questions about the CLA in Piccolo B:
1) Which communication methods exist between CLA and main CPU? The block diagrams I've seen so far only show shared memory. Is there also an interrupt mechanism, so that the CLA could trigger a CPU interrupt for certain cases? This would useful if the main CPU the data generated by CLA for further processing.
2) If the internal ADC is not accurate enough and a customer want's to use an external ADC, can they still make use of the CLA? Seems that only the internal ADC can trigger CLA. So for an external ADC I only see the workaround to use the external SOC signal and to start a dummy conversion on the internal ADC.
Thanks,
Robert