This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using TMS320F28035. I wrote my code in CLA. I don't know how to properly load CLAmathTables to Flash then copy to the CLA Data SARAM as the it said in the document.
CLASinCosTable_type0.asm doesn't seem to be automatically loaded in data RAM.
Someone posted a similary question a long time ago, but nobody answered. Here is the link to that discussion
It is urgent.
Thank you,
Max
Hi max,
the CLA tables are placed in a section "CLAmathTables". in your linker command file define the following:
CLA1mathTables : LOAD = FLASHB,
RUN = CLARAM1,
LOAD_START(_Cla1mathTablesLoadStart),
LOAD_END(_Cla1mathTablesLoadEnd),
RUN_START(_Cla1mathTablesRunStart),
LOAD_SIZE(_Cla1mathTablesLoadSize),
PAGE = 1
In your main file, before main(), you must declare these variables as follows:
extern Uint16 Cla1mathTablesLoadStart;
extern Uint16 Cla1mathTablesRunStart;
extern Uint16 Cla1mathTablesLoadSize;
In main()
memcpy(&Cla1mathTablesRunStart, &Cla1mathTablesLoadStart, (Uint32)&Cla1mathTablesLoadSize);
and you should be good to go
forgot to mention.....
note that the RUN address is CLARAM1, which is defined as
CLARAM1 : origin = 0x008C00, length = 0x000400
You need to give the CLA access to this memory in main():
Cla1Regs.MMEMCFG.bit.RAM1E = 1;
Hi Vishal,
Thank you for you reply.
I did what you suggested, and it gave a compling error:
" #169 argument of type "Uint32" is incompatible with parameter of type "Uint16"
Thank you,
Max
try this:
memcpy((Uint32 *)&Cla1mathTablesRunStart, (Uint32 *)&Cla1mathTablesLoadStart, (Uint32)&Cla1mathTablesLoadSize);
Hi Vishal,
I tried.
It now gives me the same compiling error, but two of them this time.
Thanks,
Max