This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can my currently executing application take the actions necessary to program Flash with a new version of my application which my currently executing application receives in 128 word chunks via my application's SCI interface from a custom GUI executing on a Windows PC ?
Will the Flash API need to be part of my application ?
Do I need to fill every word of the program with something "0x000" so that it does not appear as erased ("0xFFF") ?
My application that downloads the new application program from the PC and performs the flash programming will be capable of either being programmed to flash or loaded to RAM via SD emulator. When programmed to flash, my boot code copies all sections from flash to RAM and then jumps to RAM to execute the entire program from RAM. I am already able to use the emulator for the purpose of programming the application to flash or to RAM.
If the Flash API needs to be part of my application, and I program this first "reprorgamming-equipped" application to flash, it will be copied to RAM with the rest of the application and from which it will be executed when the time comes to download a new application and prorgam it to flash.
However, SPRAAQ2 specifies transferring the Flash API routines (CKFA code ?), in isolation, to RAM through the SCI under Boot ROM control. This might be appropriate in a situation where the application is not already executing, but it would not be appropriate when the application is already executing.
The flash load map appears to specify RAM loactions for switch and stack, both sections shown as uninitialized with stack as a HOLE and switch as a zero-length section (which is fine, even though I don't understand why, since I use switch/case statements). Teh flash load map appears also to specify a RAM location (0x0000d000) for the ebss section (size 0x1f3a), a RAM location (0x0000d000) for the const section (size zero), and a RAM location (0x0000f74c) for the sysmem section (size 0x0100). The peripheral file sections are also specified to be located in their usual Peripheral Frame locations.
Am I going to find everything I need for a leg up in this effort in SPRAAQ2 and the Flash API document for F28335 ? So far, I am getting re-directed to the program to flash at Boot time with ionfo that might be construed as a suggestion that my effort is going to require breaking new "risky" ground. (CSM passwords, etc.)
A fe wminutes later ...
Well, it now appears that I don't want CKFA anyway since it takes control of SCI-A, already in use by my already executing application. How would I obtain CKFA anyway ? Nothing int he Flash_API controlSUITE folders is named with CKFA in the name.
Hey Greg! Hope all is well.
First off, yes it is possible to reflash the device with 0 downtime, but it is EXTREMELY tricky. To truely do the update with 0 downtime the application needs to be able to run with no resources except for the CLA. If I remember correctly you are using a F28335 so I don't think this will be possible.
Flash API will need to be accessible to your application at some point. It could get loaded in as part of the serial stream or it could reside in your application code. One thing to remember is if you are using code security, the FlashAPI will need to be located in secure RAM when it is used.
No need to fill up unused space with 0x0000.
Ok...now to explain this SCI Flash programming...
What this guide is referring to is programming a completely blank device using SCI and the ROM bootloader. This process loads in a kernel with the flash functions (using SCI) and then loads the application code into RAM. The host side of this tool sends commands to the kernel to make calls to the flash erase and program functions. This allows you to program flash of a brand new device without JTAG. I don't think this is what you're after.
Trey
Boy you grabbed this one fast ... ! Hi, Trey. I read your posts every day and save many of them. Juudging from the dialog I think it's safe to say it's always a pleasure for us to be working with you.
When I asked if I should "fill" unused space, I should have asked if I should fill with "FFFF".
SPRAAQ2 states that this is so that CKFA can process continuous blocks of data (something that I too would like to do, anyway, I think; I dont' want to have to skip flash memory addresses while programming flash with application code binary data incoming continuously, upon request of each 128 word message, via the message stream), to provide an illegal instruction trap at those unused addresses, and to leave those unused addresses alone - unwritten/erased - while programming the flash.
When you say that the application needs to be able to run with no resources except for the Control Law Accelerator, this means no FPU, no boot.asm, etc., from the RTS library ?
And yes, Trey, it's the F28335. So, because I can't run without any "resources", I will not be able to perform a code update (write a buffer of data sitting in RAM to flash) with 0 downtime (do the writing to flash in background, non interrupt service routine, execution - my entire program runs in an interrupt), where the buffer sitting in RAM is periodically filled with incoming application code which my own SCI routine receives within the interrupt, at a byte per interrupt service ? If I wanted to write 4K of data sitting in RAM to flash, why can I not do that ?
What is meant by "FlashAPI will need to be accessed by my application at some point" ? Are you referring to the same application that I run with 0 downtime now, while not programming flash ? That I can do something with my real application doing the downloading and reprogramming short of having 0 downtime ? Or are you referring to a different application, whose sole purpose is to boot-up loading the CKFA or Flash API either to RAM (a Secure Zone if using code security) or to Flash after which it is copied to RAM via a "copy sections" asm, and to continue by downloading the real application via the CKFA and having that data written to Flash via calls to the Flash API ?
Finally, should I discard SPRAAQ2 and the Flash API document, and design this with no regard for conversion of incoming big-endian data sitting in a RAM buffer to little-endian for writing to flash, and no regard for the other special CKFA and Flash API functionality, and instead just send a byte stream into my existing real application via existing SCI interface to populate a RAM buffer and periodically memcopy the buffer into successive, adjoining blocks of Flash ? Like my colleagues do with their OMAPS ?
The F28335 FlashAPI document, on page 7, provides a list of API Do's and API Don'ts.
Among the Don'ts is " Don't execute an ISR from flash/OTP" that if the interrupt can occur during flash erase,program, or depletion recovery.
Can I execute an ISR residing in RAM even if the interrupt occurred during flash erase,program, or depletion recovery ?
Filling with 0xFFFF certainly won't hurt anything, so if it works for your application go for it.
What I mean by only use the CLA is that if you want to program flash without ANY interruption to your application the application needs to be able to run completely on the CLA. Some of our server power supply guys are requesting this because they want zero downtime during a firmware upgrade. Given that you are on the F28335 which doesn't have a CLA, I'm afraid that at some point during the upgrade the main application will have to stop. This is required because the FlashAPI code will run on the main CPU and will also disable interrupts.
You are correct, you can NOT perform a flash operation with 0 downtime. You can certainly program 4k of data sitting in RAM to flash, but the main application will have to stop for a bit to do so.
I mean that the application that you want to run with 0 downtime will make calls to the FlashAPI which will need to be located in RAM.
How you design this is up to you, but given what you want to do (0 downtime firmware update) I don't think this guide is suited to what you want to do. I would take care of any data massaging on the host to ensure that the embedded application has to do the least amount of work possible.
To answer your second post:
The guide is correct, AND....
You can execute an ISR from RAM during these flash operations, BUT several of the API calls disable interrupts so you may find your application behavior intermittent during these calls.
Trey
I get it, and in retrospect it should have been clear from the guide, that filling with ones is not a must.
"You are correct, you can NOT perform a flash operation with 0 downtime. You can certainly program 4k of data sitting in RAM to flash, but the main application will have to stop for a bit to do so."
"I mean that the application that you want to run with 0 downtime will make calls to the FlashAPI which will need to be located in RAM."
Are you aware that my entire application, executes from RAM ?
In fact, after initialization, everything executes from within a 40KHz interrupt, everything that is not included in Main's background loop, which is nothing at this time. But I had planned to take my incoming message buffer and copy it to flash while executing in the background. Why would te main application have to be stopped for a bit to program a 4K buffer sitting in RAM to flash ? Because even the programming of a block that size takes longer then the time between 40KHz interrupts (25usec, 3750 CPU ticks), which would be the maximum time available to the background, if I did nothing in my ISR ?
Is there a minimum size that has to be programmed, or only a minimum size (a sector) that has to be erased ?
The data coming from the host will apparently have to be a BIN file produced by the COFF to Hex converters as specified in the Guide and the FlashAPI documents. The expectation is that the incoming data would be deposited in a buffer that would be transferred as is to flash. I get what you are saying, I think: that any endianness issues should be pre-compensated for on the host side. Does the converter's outputs have to be pre-conditioned ? I did not pull that endianness question out of thin air but saw it mentioned in one of the documents or in a code snippet or something.
And since my last post I had finally read some of the FlashAPI document for the F28335 where there is an indication that interrupts are disabled during flash operations. I was not sure how absolute this statement is. But now, after re-reading it I am getting more certain that it is absolute. The uncertainty arises from the statement in Step 9 (which corresponds with Section 14), an Optional step for my application to perform before calling any API Function, that the application can optionally disable global interrupts before calling an API function. Then the description of what the API function will do includes the statement that the API function performs the called operation and then disables and restores global interrupts around the critical code segments. So, it performs the called operation and then disables and restores interrupts. Makes no sense to disable/enable after performing the called API function. So I guess what is meant (is it ?) is that the API function is called; the API function executes some stuff before getting to a critical section; the API function disabled interrupts, the API function executes critical stuff, the API function enables interrupts, the API function executes some more uncritical stuff after interrupts are disabled, the API function terminates. And none of that is executed by the user, much less optionally. And yet, even though the API function(s) (which ones ?) will disable interrupts itself, the application may do it in advance anyway. Why ? Just a long term disable for the entire erase/program/verify duration, for those who are not looking to minimize down time ?
Are the API Library components' source code available ?
Hello everyone,
I am in the exact same case that Greg describes. My main application resides in flash memory and I have couple time-critical functions residing in SARAM. A host computer communicates with the DSP via SCIA and I want to implement an on-field firmware upgrade via SCIA. My SCIA functions are located in SARAM, interrupt based and use FIFO.
I have read the Flash API documentation from controlSUITE and I want to make sure that I have understand everything here is the sequence I should follow :
I have couple questions:
Is this approach correct ?
Can I use safely my SCIA functions since they are interrupt based (FIFO) ?
Any comments are welcome. Thanks for your help.
Cedric,
For the most part this approach is correct and will work.