Hello,
I am using the schematic design of Concerto Control Card t get idea about boot mode design.
In the design of Concerto Control Card, USB to JTAG/UART is used to provide isolated JTAG. In this design, UAR/SCI on PE5_GPIO29 and PE4_GPIO28 are used to provide code loading.
However, it is confusing for me. Because based on datasheet and also Concerto F28M35x Technical Reference Manual, if we want to have boot from UART we should use PA0_GPIO0 and PA1_GPIO1. Also for boot from SCI we should use PF3_GPIO35 and PF4_GPIO36.
I will appreciate if someone clarifies this for me,
Thanks in advance,
Best regards,
Masoud Zamani.