This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi;
I have a ISR that used to collect data from the SCI interface RX data; my ISR should collect packet of data, and if it a valid one, allocate a memory for the packet, so the "main" can parse the incoming the data and then free the memory….
The problem is that when the first time the ISR is running it really allocates the memory space, but in the second time malloc return NULL pointer.
Firstly I thought that I don’t have enough space in the heap, so I resize it to 0x800, but did doesn't solve my problem…
So what do you think? What seems to be the thing I do thaw wrong way?
P.S:
A part of my code:
interrupt void SciaRxIsr(void)
{
volatile RxPacket *rx_packet;
Uint16 rx_byte;
static char rx_buffer[MAX_PACKET_SIZE];
static int rx_buffer_index = 0;
static Rx_Fsm fsm_curr_state = Wait_For_Stx_State;
rx_byte = SciaRegs.SCIRXBUF.bit.RXDT;
// if no frame error occurred and no parity error occurred
if((SciaRegs.SCIRXBUF.bit.SCIFFFE & SciaRegs.SCIRXBUF.bit.SCIFFPE) == 0)
{
// Verifying ETX at the end of the packet
case Wait_For_Etx_State:
{
if(rx_byte == ETX) // Read ETX
{
//add rx buffer to linked list
rx_packet = (RxPacket*)malloc(sizeof(RxPacket));
if(rx_packet == NULL)
{
// Node creation failed
fsm_curr_state = Wait_For_Stx_State;
}
else
{
// Allocate space for the command data
rx_packet->command_data = (char*)malloc(sizeof(rx_buffer[0]));
if(rx_packet->command_data == NULL)
{
// Node creation failed
fsm_curr_state = Wait_For_Stx_State;
}
}
SciaRegs.SCIFFRX.bit.RXFFOVRCLR = 1; // Clear Overflow flag
SciaRegs.SCIFFRX.bit.RXFFINTCLR = 1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all |= 0x100; // Issue PIE ack
}
Hi Igor,
Thanks for your quick answer.
But the thing is that I want to create a linked list.
The ISR should add items to the list and the main will remove items from the list.
.
Hi!
I don't see some problem. You can create the function for a work with a linked list through a pointer to allocated memory area. This function you can call into ISR. The pointer should to be passed as a parameter.
Regards,
Igor