This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28375D: Can only malloc(1) once before malloc fails

Part Number: TMS320F28375D


Tool/software: TI C/C++ Compiler

Hi,

I am trying to create a cpp object but new fails when trying to malloc. After a bit of digging around, I figured out malloc is failing at  

   if (size > heap_size()) in memory.c

I changed my heap size from 0x250 to 0x800 (using the --heap_size flag under properties->CCS Build->Linker->Basic Options) but I am still not able to malloc.

From some more testing, I noticed I can only get malloc to pass if I ask for 1 memory location (malloc(1)). If I try to malloc(1) twice or malloc any other value other than 1, malloc fails.

I checked the memory browser at the pointer returned by the only malloc that passed and it seemed like there was plenty of unused memory (all zeros).

I'm including the cmd file because I believe it has something to do with the linker file or a compilation/linking setting that is off.

Please Help,

Thanks,

Miguel

#ifdef CLA_C
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C


MEMORY
{
   /* BEGIN is used for the "boot to Flash" bootloader mode   */
   BEGIN            : origin = 0x080000, length = 0x000002
   BOOT_RSVD        : origin = 0x000002, length = 0x0001AE     /* Part of M0, BOOT rom will use this for stack */
   RAMM0            : origin = 0x0001B0, length = 0x000250
   RAMM1            : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
// RAMD0            : origin = 0x00C000, length = 0x000800
// RAMD1            : origin = 0x00C800, length = 0x000800
   RAMD0_1          : origin = 0x00C000, length = 0x001000
   RAMLS0           : origin = 0x008000, length = 0x001000
//   RAMLS0           : origin = 0x008000, length = 0x000800
//   RAMLS1           : origin = 0x008800, length = 0x000800
   RAMLS2           : origin = 0x009000, length = 0x000800
   RAMLS3           : origin = 0x009800, length = 0x000800
   RAMLS4           : origin = 0x00A000, length = 0x000800
   RAMLS5           : origin = 0x00A800, length = 0x000800
   RAMLS6           : origin = 0x00B000, length = 0x000800
   RAMLS7           : origin = 0x00B800, length = 0x000800

   RAMGS0           : origin = 0x00D000, length = 0x005000
//   RAMGS0           : origin = 0x00D000, length = 0x001000
//   RAMGS1           : origin = 0x00E000, length = 0x001000
//   RAMGS2           : origin = 0x00F000, length = 0x001000
//   RAMGS3           : origin = 0x010000, length = 0x001000

//   RAMGS_4           : origin = 0x011000, length = 0x004000

//   RAMGS4           : origin = 0x011000, length = 0x001000
   RAMGS5           : origin = 0x012000, length = 0x004000
//   RAMGS5           : origin = 0x012000, length = 0x001000
//   RAMGS6           : origin = 0x013000, length = 0x001000
//   RAMGS7           : origin = 0x014000, length = 0x001000
//   RAMGS8           : origin = 0x015000, length = 0x001000
   RAMGS9           : origin = 0x016000, length = 0x001000
   RAMGS10          : origin = 0x017000, length = 0x006000
//   RAMGS10          : origin = 0x017000, length = 0x001000
//   RAMGS11          : origin = 0x018000, length = 0x001000
//   RAMGS12          : origin = 0x019000, length = 0x001000
//   RAMGS13          : origin = 0x01A000, length = 0x001000
//   RAMGS14          : origin = 0x01B000, length = 0x001000
//   RAMGS15          : origin = 0x01C000, length = 0x001000

   /* Flash sectors */
   FLASHA           : origin = 0x080002,   length = 0x001FFE	/* on-chip Flash */
   FLASHB           : origin = 0x082000,   length = 0x002000	/* on-chip Flash */
   FLASHC           : origin = 0x084000,   length = 0x002000	/* on-chip Flash */
   FLASHD           : origin = 0x086000,   length = 0x002000	/* on-chip Flash */
   FLASHE           : origin = 0x088000,   length = 0x008000	/* on-chip Flash */
   FLASHF           : origin = 0x090000,   length = 0x008000	/* on-chip Flash */
   FLASHG           : origin = 0x098000,   length = 0x008000	/* on-chip Flash */
   FLASHH           : origin = 0x0A0000,   length = 0x008000	/* on-chip Flash */
   FLASHI           : origin = 0x0A8000,   length = 0x008000	/* on-chip Flash */
   FLASHJ           : origin = 0x0B0000,   length = 0x008000	/* on-chip Flash */
   FLASHK           : origin = 0x0B8000,   length = 0x002000	/* on-chip Flash */
   FLASHL           : origin = 0x0BA000,   length = 0x002000	/* on-chip Flash */
   FLASHM           : origin = 0x0BC000,   length = 0x002000	/* on-chip Flash */
   FLASHN           : origin = 0x0BE000,   length = 0x002000	/* on-chip Flash */

   CPU1TOCPU2RAM   : origin = 0x03A000, length = 0x000800
   CPU2TOCPU1RAM   : origin = 0x03B000, length = 0x000800

   CANA_MSG_RAM     : origin = 0x049000, length = 0x000800
   CANB_MSG_RAM     : origin = 0x04B000, length = 0x000800

   RESET            : origin = 0x3FFFC0, length = 0x000002

   CLA1_MSGRAMLOW   : origin = 0x001480,   length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500,   length = 0x000080
}

SECTIONS
{
   codestart           : > BEGIN, ALIGN(4)
   .text               : >> FLASHB | FLASHH | FLASHI | FLASHJ | FLASHK | FLASHL | FLASHM | FLASHN, ALIGN(4)
   .cinit              : > FLASHG, ALIGN(4)
//   .cinit              : > RAMLS1, ALIGN(4)
   .switch             : > FLASHG, ALIGN(4)
   .reset              : > RESET, TYPE = DSECT /* not used, */
   .stack              : > RAMM1
   DMARAML4 		   : > RAMM0, PAGE = 0

#if defined(__TI_EABI__)

   .init_array      : > FLASHG, ALIGN(8)
   .bss             : > RAMGS0 , ALIGN(4)
   .bss:output      : > RAMLS0, ALIGN(4)
   .bss:cio         : > RAMLS0
   .data            : > RAMLS0
   .sysmem          : > RAMLS0
   /* Initalized sections go in Flash */
   .const           : > FLASHG, ALIGN(8)
#else
   .pinit           : > RAMLS0 , ALIGN(8)
//   .pinit           : > FLASHG, ALIGN(8)
//   .ebss            : > RAMGS5
   .ebss            : > RAMGS0

//   .ebss            : > RAMLS0 , ALIGN(4)
//   .esysmem         : > RAMGS10 , ALIGN(8)
   .esysmem         : > RAMLS6 | RAMLS7 , ALIGN(8)

   .cio             : > RAMLS6 | RAMLS7 , ALIGN(8)
   /* Initalized sections go in Flash */
   .econst          : > FLASHG, ALIGN(8)
#endif


   /* Flash Programming Buffer */
   BufferDataSection : > RAMLS5,  ALIGN(8)


   MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, type=NOINIT
   MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, type=NOINIT

    /* CLA specific sections */
#if defined(__TI_EABI__)
   Cla1Prog         :   LOAD = FLASHF,
                        RUN = RAMLS4 | RAMLS5,
                        LOAD_START(Cla1funcsLoadStart),
                        LOAD_END(Cla1funcsLoadEnd),
                        RUN_START(Cla1funcsRunStart),
                        LOAD_SIZE(Cla1funcsLoadSize),
                        ALIGN(8)
#else
   Cla1Prog         :   LOAD = FLASHF,
                        RUN = RAMLS4 | RAMLS5,
                        LOAD_START(_Cla1funcsLoadStart),
                        LOAD_END(_Cla1funcsLoadEnd),
                        RUN_START(_Cla1funcsRunStart),
                        LOAD_SIZE(_Cla1funcsLoadSize),
                        ALIGN(8)
#endif
   ClaData			: > RAMLS3


#ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 15009000

        #if defined(__TI_EABI__)

    GROUP { .TI.ramfunc  { -l F021_API_F2837xD_FPU32.lib} }
            LOAD = FLASHD,
			 RUN = RAMD0_1 | RAMGS5,
			 LOAD_START(RamfuncsLoadStart),
			 LOAD_SIZE(RamfuncsLoadSize),
			 LOAD_END(RamfuncsLoadEnd),
			 RUN_START(RamfuncsRunStart),
			 RUN_SIZE(RamfuncsRunSize),
			 RUN_END(RamfuncsRunEnd),
			 PAGE = 0, ALIGN(8)
        #else


    GROUP { .TI.ramfunc  { -l F021_API_F2837xD_FPU32.lib} }
            LOAD = FLASHD,
			 RUN = RAMD0_1 | RAMGS5,

			 LOAD_START(_RamfuncsLoadStart),
			 LOAD_SIZE(_RamfuncsLoadSize),
			 LOAD_END(_RamfuncsLoadEnd),
			 RUN_START(_RamfuncsRunStart),
			 RUN_SIZE(_RamfuncsRunSize),
			 RUN_END(_RamfuncsRunEnd),
			 PAGE = 0, ALIGN(8)

        #endif

    #else
    	GROUP { ramfuncs { -l F021_API_F2837xD_FPU32.lib} }
                LOAD = FLASHD,
//			 	RUN = RAMLS0,
			 RUN = RAMD0_1,
				 LOAD_START(_RamfuncsLoadStart),
				 LOAD_SIZE(_RamfuncsLoadSize),
				 LOAD_END(_RamfuncsLoadEnd),
				 RUN_START(_RamfuncsRunStart),
				 RUN_SIZE(_RamfuncsRunSize),
				 RUN_END(_RamfuncsRunEnd),
				 PAGE = 0, ALIGN(8)
    #endif
#endif



   Cla1ToCpuMsgRAM  : > CLA1_MSGRAMLOW, type=NOINIT
   CpuToCla1MsgRAM  : > CLA1_MSGRAMHIGH, type=NOINIT

   /* SFRA specific sections */
   SFRA_F32_Data	: > RAMGS9, ALIGN = 64

#ifdef CLA_C

   /* CLA C compiler sections */
   //
   // Must be allocated to memory the CLA has write access to
   //
   CLAscratch       :
                     { *.obj(CLAscratch)
                     . += CLA_SCRATCHPAD_SIZE;
                     *.obj(CLAscratch_end) } >  RAMLS2


   .scratchpad      : > RAMLS2
   .bss_cla         : > RAMLS2


#if defined(__TI_EABI__)
   .const_cla       :   LOAD = FLASHF,
                        RUN = RAMLS6,

                        RUN_START(Cla1ConstRunStart),
                        LOAD_START(Cla1ConstLoadStart),
                        LOAD_SIZE(Cla1ConstLoadSize),
                        ALIGN(8)
#else
   .const_cla       :   LOAD = FLASHF,
                        RUN = RAMLS6,
                        RUN_START(_Cla1ConstRunStart),
                        LOAD_START(_Cla1ConstLoadStart),
                        LOAD_SIZE(_Cla1ConstLoadSize),
                        ALIGN(8)
#endif
#endif //CLA_C

   /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU1TOCPU2RAM
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }

    GROUP : > CPU2TOCPU1RAM
    {
        GETBUFFER :    TYPE = DSECT
        GETWRITEIDX :  TYPE = DSECT
        PUTREADIDX :   TYPE = DSECT
    }

}

  • Please look in the linker map file for the symbol __SYSMEM_SIZE.  What is the value of this symbol?

    Thanks and regards,

    -George

  • abs   00000800  __SYSMEM_SIZE       

    Also, I ran

       size_t totalSizeAvaliable =  __TI_heap_total_available();
       size_t largestAvaliable=  __TI_heap_largest_available();

    and got

    totalSizeAvaliable = 2

    largestAvaliable = 2

  • Something odd is happening.  Please try another experiment.

    The compiler installation includes a standalone disassembler named dis2000.  It is in the same \bin directory as the compiler cl2000.  A typical directory path is ...

    C:\ti\ccs1011\ccs\tools\compiler\ti-cgt-c2000_20.2.1.LTS\bin

    From the command line run a command similar to ...

    % dis2000 project_executable_file.out > dis.txt

    Inspect the text file dis.txt.  Search for the function named memalign.  You will see something similar to ...

    000001e7        _aligned_alloc:
    000001e7        _memalign:
    000001e7   b2bd   MOVL         *SP++, XAR1
    000001e8   aabd   MOVL         *SP++, XAR2
    000001e9   a2bd   MOVL         *SP++, XAR3
    000001ea   fe02   ADDB         SP, #2
    000001eb   864c   MOVL         XAR2, *-SP[12]
    000001ec   8ba9   MOVL         XAR1, ACC
    000001ed   aaa9   MOVL         ACC, XAR2
    000001ee   6111   SB           17, EQ
    000001ef   28a9   MOV          AL, #0x0800
    000001f0   0800
    

    The first column is the address.  Your addresses will be different.  But everything else should be similar.  The important detail is the constant 0x800 at the end.  This is the size of the heap encoded in the program.  Do you see the same thing?  Or something else?  

    If you see 0x800 in the disassembly, then here is a further step. Load the program without running it.  Check the address that should contain 0x800.  Does it?  Set a breakpoint at the start of memalign, then run to it.  Does this location still contain 0x800?

    Please let me know what you see.

    Thanks and regards,

    -George

  • Hi George,

    I was able to work around the issue by increasing the heap size to 0x1000. Now I have 0x700 ish space in my heap so malloc and new are working.

    I have a major deadline this week, so I'll wait to try out your test until next week.

    Thanks,

    Miguel

  • OK.  I plan on hearing from you next week.

    Thanks and regards,

    -George