Other Parts Discussed in Thread: TMS320F28235
I encountered a problem with ADCRESULT registers on C2000 TMS320F28235.
When I use AdcRegs.ADCRESULTx, there is no problem, just requiring >>4 bits to get the correct value.
When I tried using AdcMirror.ADCRESULTx, the result was not what I expected.
For example, I did ADC conversion from ch0 to ch15, using sequence mode, 8 samples for each channel per sequence.
The result looks like,
(ch00)1514, 1515, 1515, 1516, 1515, 1515, 1514, 1514
(ch01)2585, 2585, 2584, 2584, 2584, 2584, 2584, 2585
(ch02)10, 12, 13, 14, 14, 14, 14, 14
(ch03)12, 14, 14, 15, 15, 15, 16, 15
(ch04)14, 15, 17, 17, 17, 19, 17, 18
(ch05)14, 15, 16, 17, 18, 18, 17, 18
(ch06)12, 14, 16, 16, 16, 16, 17, 17
(ch07)1486, 1487, 1487, 1488, 1487, 1488, 1487, 1487
(ch08)0, 16, 17, 17, 17, 17, 17, 17
(ch09)15, 561, 561, 561, 560, 561, 561, 561
(ch10)561, 14, 15, 15, 15, 16, 15, 15
(ch11)16, 14, 15, 15, 16, 16, 15, 15
(ch12)15, 15, 16, 15, 15, 16, 15, 15
(ch13)15, 14, 15, 16, 15, 16, 15, 15
(ch14)15, 14, 15, 15, 15, 16, 15, 15
(ch15)14, 15, 15, 15, 16, 15, 15, 14
ch08 is connected to DC supply (0V output), ch09 is connected with an amp circuit, ch10 is connected to GND.
The first ADC result of ch09 and ch10 was not correct. I tried many times and reset the board, the problem was still there.
Another example is like,
(ch08)14, 15, 16, 16, 16, 17, 17, 18
(ch09)15, 2344, 2344, 2345, 2344, 2343, 2344, 2344
(ch10)2345, 15, 15, 15, 15, 15, 15, 15
The problem only occurred on ch09 and ch10, sequence mode.
Using AdcRegs.ADCRESULTx has no problem.
Using Cascaded mode has no problem.
Unfortunately, now the problem disappeared! I am not able to reproduce the problem now.
Though I can use AdcRegs.ADCRESULTx instead of the mirror ones, I want to know the root cause.
Any replies appreciated.
Piece of my code.
(All ADC registers are using default values, ADC_cal() is called after reset.)
(CLKIN=25MHz, HSPCLK=CLKIN, ADCCLK=HSPCLK.)
Uint16 DSP_Adc_Seq(Uint16 channel, Uint16 nConv, Uint16* resbuf)
{
Uint16 i, adval, adsum;
volatile Uint16* pAdcResult;
Uint16 SeqId;
if (channel < 8)
SeqId = 0;
else
SeqId = 1;
pAdcResult = &AdcMirror.ADCRESULT0;
//pAdcResult = &AdcRegs.ADCRESULT0;
if (SeqId > 0)
pAdcResult += 8;
nConv = 8;
if (SeqId==0) //Seq1...
{
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;
AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = nConv - 1;
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = channel; //
if (nConv > 1)
AdcRegs.ADCCHSELSEQ1.bit.CONV01 = channel;
if (nConv > 2)
AdcRegs.ADCCHSELSEQ1.bit.CONV02 = channel;
if (nConv > 3)
AdcRegs.ADCCHSELSEQ1.bit.CONV03 = channel;
if (nConv > 4)
AdcRegs.ADCCHSELSEQ2.bit.CONV04 = channel;
if (nConv > 5)
AdcRegs.ADCCHSELSEQ2.bit.CONV05 = channel;
if (nConv > 6)
AdcRegs.ADCCHSELSEQ2.bit.CONV06 = channel;
if (nConv > 7)
AdcRegs.ADCCHSELSEQ2.bit.CONV07 = channel;
if (nConv > 8)
AdcRegs.ADCCHSELSEQ3.bit.CONV08 = channel;
if (nConv > 9)
AdcRegs.ADCCHSELSEQ3.bit.CONV09 = channel;
if (nConv > 10)
AdcRegs.ADCCHSELSEQ3.bit.CONV10 = channel;
if (nConv > 11)
AdcRegs.ADCCHSELSEQ3.bit.CONV11 = channel;
if (nConv > 12)
AdcRegs.ADCCHSELSEQ4.bit.CONV12 = channel;
if (nConv > 13)
AdcRegs.ADCCHSELSEQ4.bit.CONV13 = channel;
if (nConv > 14)
AdcRegs.ADCCHSELSEQ4.bit.CONV14 = channel;
if (nConv > 15)
AdcRegs.ADCCHSELSEQ4.bit.CONV15 = channel;
}
else //Seq2...
{
AdcRegs.ADCTRL2.bit.RST_SEQ2 = 1;
AdcRegs.ADCMAXCONV.bit.MAX_CONV2 = nConv - 1;
AdcRegs.ADCCHSELSEQ3.bit.CONV08 = channel;
if (nConv > 1)
AdcRegs.ADCCHSELSEQ3.bit.CONV09 = channel;
if (nConv > 2)
AdcRegs.ADCCHSELSEQ3.bit.CONV10 = channel;
if (nConv > 3)
AdcRegs.ADCCHSELSEQ3.bit.CONV11 = channel;
if (nConv > 4)
AdcRegs.ADCCHSELSEQ4.bit.CONV12 = channel;
if (nConv > 5)
AdcRegs.ADCCHSELSEQ4.bit.CONV13 = channel;
if (nConv > 6)
AdcRegs.ADCCHSELSEQ4.bit.CONV14 = channel;
if (nConv > 7)
AdcRegs.ADCCHSELSEQ4.bit.CONV15 = channel;
}
// Start SEQ1/SEQ2
if (SeqId==0)
AdcRegs.ADCTRL2.bit.SOC_SEQ1 = 1;// Enable SOCA from SW to start SEQ1
else
AdcRegs.ADCTRL2.bit.SOC_SEQ2 = 1;// Enable SOCB from SW to start SEQ2
// Wait ADC conv completion.
while (1)
{
if (SeqId==0)
{
if ( !AdcRegs.ADCST.bit.SEQ1_BSY )
break;
}
else
{
if ( !AdcRegs.ADCST.bit.SEQ2_BSY )
break;
}
}
adsum = 0;
for(i=1; i<nConv; i++)
{
adval = pAdcResult[i];
if (resbuf)
resbuf[i] = adval; // Copy adc results to buffer
adsum += adval;
}
adval = adsum / nConv;
if (SeqId==0)
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1;
else
AdcRegs.ADCST.bit.INT_SEQ2_CLR = 1;
return adval;
}