This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using the Piccolo F28069 and trying to do the usual loading of code to RAM using ramfunc. I ran into an issue when trying to run without the emulator (stand alone mode).
Everything works fine until the code size in RAM exceeds a certain limit, in this case it is 0x03d8. Then it would not run in stand alone mode (still can run with an emulator though). I tried to comment out a few lines of code that are supposed to be in RAM and it was back to working again (stand alone). I've looked at the map file and nothing looked out of the ordinary. All the intended functions are located in RAM as they are supposed to, and there is still plenty of memory available after all the ramfunc code. I've never seen this before and wonder if anyone has a clue. Probably something simple that I overlooked.
Thanks,
Erik
Hi Erik!
Erik Dinh said:I am using the Piccolo F28069 and trying to do the usual loading of code to RAM using ramfunc. I ran into an issue when trying to run without the emulator (stand alone mode).
At first. Do you mean that you don't use loading to flash (only to RAM)? In fact at this case the firmware will not start in standalone mode of DSP.
Regards,
Igor
Hi Igor,
I used the FLASH cmd file if that was what you meant. If you read further you'd see that my code runs standalone until I exceed about 1k of code in RAM.
This is one line of code in the map file that shows the status of the RAM code
origin length used unused
PRAML0 00008000 00000800 000003c9 00000437 RWIX <- not working standalone
When I comment out one line of code that is supposed to be in RAM this looks like
PRAML0 00008000 00000800 000003b8 00000448 RWIX <- back to working standalone
(Notice the difference in "used" memory).
Any idea would be appreciated.
Erik
Hi Erik!
Erik Dinh said:When I comment out one line of code that is supposed to be in RAM this looks like
PRAML0 00008000 00000800 000003b8 00000448 RWIX <- back to working standalone
Does it refer to a some particular line or to any one line?
Also I would recommend you the following:
5773.TI_Running_from_Flash_spra958l.pdf
3808.TI_Copying Compiler Sections From Flash to RAM.pdf
http://processors.wiki.ti.com/index.php/C28x_Compiler_-_Understanding_Linking
Regards,
Igor
Erik,
I once faced a similar issue upon flashing,which was that i was able to flash my program to DSP successfully until my code size of program was too large to fit into internal ram , the solution was to move those unfit-able sections to external RAM, although I am not sure if you are facing same issues, just for your reference.
Regards,
Zachary
Igor,
No, it doesn't matter what line of RAM code I comment out, as long as it brings the "used" memory down a bit, and it is back to working stand alone. This is very strange to me.
Zachary,
I have no problem with space. If you look at the line on my map file above, you'll see that I still have "unused" space left.
Btw, I am using the F28069 Control Card.
Again, any help would be appreciated.
Erik
Here is the CMD file. And yes I am familiar with the documents you referenced.
/* //########################################################################### // // FILE: F28069_FLASH.CMD // // TITLE: Linker Command File For F28069 Device Flash API // //########################################################################### // $TI Release: F2806x Flash API Release V1.00 $ // $Release Date: March 31, 2011 $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // // The header linker files are found in <base>\F2806x_headers\cmd // // For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd ========================================================= */ /* Define the memory block start/length for the F2806x PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F2806x are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. Contiguous SARAM memory blocks can be combined if required to create a larger memory block. */ MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ PRAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */ OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */ FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */ FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */ FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */ FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */ FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */ FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */ FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL_PROG: origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */ IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ DRAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */ DRAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ DRAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */ DRAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */ DRAML4 : origin = 0x00A000, length = 0x002000 /* on-chip RAM block L4 */ DRAML5 : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L5 */ DRAML6 : origin = 0x00E000, length = 0x002000 /* on-chip RAM block L6 */ DRAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */ DRAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */ FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */ } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /* Allocate program areas: */ /* The Flash API functions can be grouped together as shown below. The defined symbols _Flash28_API_LoadStart, _Flash28_API_LoadEnd and _Flash28_API_RunStart are used to copy the API functions out of flash memory and into SARAM */ /******************************************************************/ /* For Piccolo we dont need to copy the API from Flash as it is */ /* present in BOOT ROM */ /******************************************************************/ /* Flash28_API: // Applicable only when API is not in BootROM { -lFlash2802x_API_V100a.lib(.text) } LOAD = FLASHD, RUN = PRAML0, LOAD_START(_Flash28_API_LoadStart), LOAD_END(_Flash28_API_LoadEnd), RUN_START(_Flash28_API_RunStart), PAGE = 0 */ .cinit : > FLASHA PAGE = 0 .pinit : > FLASHA, PAGE = 0 .text : > FLASHA PAGE = 0 codestart : > BEGIN PAGE = 0 ramfuncs : LOAD = FLASHA, RUN = PRAML0, LOAD_START(_RamfuncsLoadStart), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), PAGE = 0 csmpasswds : > CSM_PWL_PROG PAGE = 0 csm_rsvd : > CSM_RSVD PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > DRAMM0 PAGE = 1 .ebss : > DRAML4 PAGE = 1 .esysmem : > DRAML4 PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASHA PAGE = 0 .switch : > FLASHA PAGE = 0 /* Allocate IQ math areas: */ IQmath : > FLASHA PAGE = 0 /* Math Code */ IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNexpTable.obj> (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNasinTable.obj> (IQmathTablesRam) } */ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT } /* //=========================================================================== // End of file. //=========================================================================== */
Here is the CMD file. And yes I am familiar with the documents you referenced.
/* //########################################################################### // // FILE: F28069_FLASH.CMD // // TITLE: Linker Command File For F28069 Device Flash API // //########################################################################### // $TI Release: F2806x Flash API Release V1.00 $ // $Release Date: March 31, 2011 $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // // The header linker files are found in <base>\F2806x_headers\cmd // // For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd ========================================================= */ /* Define the memory block start/length for the F2806x PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F2806x are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. Contiguous SARAM memory blocks can be combined if required to create a larger memory block. */ MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ PRAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */ OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */ FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */ FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */ FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */ FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */ FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */ FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */ FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL_PROG: origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */ IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ DRAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */ DRAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ DRAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */ DRAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */ DRAML4 : origin = 0x00A000, length = 0x002000 /* on-chip RAM block L4 */ DRAML5 : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L5 */ DRAML6 : origin = 0x00E000, length = 0x002000 /* on-chip RAM block L6 */ DRAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */ DRAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */ FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */ } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /* Allocate program areas: */ /* The Flash API functions can be grouped together as shown below. The defined symbols _Flash28_API_LoadStart, _Flash28_API_LoadEnd and _Flash28_API_RunStart are used to copy the API functions out of flash memory and into SARAM */ /******************************************************************/ /* For Piccolo we dont need to copy the API from Flash as it is */ /* present in BOOT ROM */ /******************************************************************/ /* Flash28_API: // Applicable only when API is not in BootROM { -lFlash2802x_API_V100a.lib(.text) } LOAD = FLASHD, RUN = PRAML0, LOAD_START(_Flash28_API_LoadStart), LOAD_END(_Flash28_API_LoadEnd), RUN_START(_Flash28_API_RunStart), PAGE = 0 */ .cinit : > FLASHA PAGE = 0 .pinit : > FLASHA, PAGE = 0 .text : > FLASHA PAGE = 0 codestart : > BEGIN PAGE = 0 ramfuncs : LOAD = FLASHA, RUN = PRAML0, LOAD_START(_RamfuncsLoadStart), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), PAGE = 0 csmpasswds : > CSM_PWL_PROG PAGE = 0 csm_rsvd : > CSM_RSVD PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > DRAMM0 PAGE = 1 .ebss : > DRAML4 PAGE = 1 .esysmem : > DRAML4 PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASHA PAGE = 0 .switch : > FLASHA PAGE = 0 /* Allocate IQ math areas: */ IQmath : > FLASHA PAGE = 0 /* Math Code */ IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNexpTable.obj> (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNasinTable.obj> (IQmathTablesRam) } */ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT } /* //=========================================================================== // End of file. //=========================================================================== */
Hi Erik!
At first try this
/* //########################################################################### // // FILE: F28069_FLASH.CMD // // TITLE: Linker Command File For F28069 Device Flash API // //########################################################################### // $TI Release: F2806x Flash API Release V1.00 $ // $Release Date: March 31, 2011 $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // // The header linker files are found in <base>\F2806x_headers\cmd // // For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd ========================================================= */ /* Define the memory block start/length for the F2806x PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F2806x are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. Contiguous SARAM memory blocks can be combined if required to create a larger memory block. */ MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ PRAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */ OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */ FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */ FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */ FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */ FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */ FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */ FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */ FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL_PROG: origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */ IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ DRAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */ DRAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ DRAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */ DRAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */ DRAML4 : origin = 0x00A000, length = 0x002000 /* on-chip RAM block L4 */ DRAML5 : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L5 */ DRAML6 : origin = 0x00E000, length = 0x002000 /* on-chip RAM block L6 */ DRAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */ DRAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */ FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */ } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /* Allocate program areas: */ /* The Flash API functions can be grouped together as shown below. The defined symbols _Flash28_API_LoadStart, _Flash28_API_LoadEnd and _Flash28_API_RunStart are used to copy the API functions out of flash memory and into SARAM */ /******************************************************************/ /* For Piccolo we dont need to copy the API from Flash as it is */ /* present in BOOT ROM */ /******************************************************************/ /* Flash28_API: // Applicable only when API is not in BootROM { -lFlash2802x_API_V100a.lib(.text) } LOAD = FLASHD, RUN = PRAML0, LOAD_START(_Flash28_API_LoadStart), LOAD_END(_Flash28_API_LoadEnd), RUN_START(_Flash28_API_RunStart), PAGE = 0 */ .cinit : > FLASHA PAGE = 0 .pinit : > FLASHA, PAGE = 0 .text : > FLASHC PAGE = 0 codestart : > BEGIN PAGE = 0 ramfuncs : LOAD = FLASHD, RUN = PRAML0, LOAD_START(_RamfuncsLoadStart), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), PAGE = 0 csmpasswds : > CSM_PWL_PROG PAGE = 0 csm_rsvd : > CSM_RSVD PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > DRAMM0 PAGE = 1 .ebss : > DRAML4 PAGE = 1 .esysmem : > DRAML4 PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASHA PAGE = 0 .switch : > FLASHA PAGE = 0 /* Allocate IQ math areas: */ IQmath : > FLASHA PAGE = 0 /* Math Code */ IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNexpTable.obj> (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNasinTable.obj> (IQmathTablesRam) } */ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT } /* //=========================================================================== // End of file. //=========================================================================== */
Regards,
Igor
Hi Erik!
Honestly I didn't find something wrong in your CMD so far. Just I have tried to go empiric way. What kind of emulator do you apply?
Regards,
Igor
I use CCS 5.4. I've tried on 2 different control cards and they both showed the same symptom. I've also tried different RAM blocks but it didn't help either. Just a reminder I can run code with the emulator. Only when I try running on its own then I'd have this issue.
For now as a temporary fix I am running most code from FLASH, but I'd like to find the solution so I can get back some processing time (by running some code in RAM).
Thanks again,
Well...Just in case I would try to test this issue. One might take some simple example (for example Blinky from controlSUITE) and define array:
#pragma DATA_SECTION( array,"section name")
Uint16 array[N];
One might try N up to 2048 (0x800) and check when the project will behave like your project (if of course it's going to happen ...). Maybe the some problem with the code is somehow linked to its size in memory...Of course it sounds absurd.
Regards,
Igor
Hi Erik!
There are a couple of suggestions also.
1 Reinstalling CCSv5.4
2 To try CCSv5.2
Regards,
Igor
Hi Igor,
Your first suggestion: I am not sure about creating the data array because I have problem with the program space, not data space. However, I can create some fake code to put in RAM instead and see how it goes.
About the second suggestion: I am a bit confused about your wording. Can you clarify that I need to "Uninstall 5.4" and install 5.2? If so, are you sure 5.2 will resolve it? It is a major undertaking with high risk of messing up other things and I don't feel like I have time to experiment with this if the outcome is not certain.
Thanks,
Erik
Hi Erik!
1) Yes, I understand that there is issue of program memory (not data memory), but I would try anyway. In my opinion this will help to locate the reason issue.
2) I mean to uninstall CCSv5.4 and install it again. If this step will not help then to try to go on CCSv5.2. (If you pay attention on threads of CCS forum you will see that some problems with v5.4 occur sometimes).
Regards,
Igor
Just an update,
After having tried various paths to fix the issue, I took a look at the actual MemCopy function (given by one of the examples in controlSuite) and replaced it with the memcpy function. It works! I don't have time at the moment to find out the reason but the bottom line is:
Do not use this!
void Example_MemCopy(Uint16 *SourceAddr, Uint16* SourceEndAddr, Uint16* DestAddr)
{
while(SourceAddr < SourceEndAddr)
{
*DestAddr++ = *SourceAddr++;
}
return;
}
Use this
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
Thanks for all the feedback;
Erik