This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using graphs in CCS4

Hi all,

I'm having problems using the graph tool in CCSv4. I'm currently working with the "Sensorless FOC PMSM" with a F28335. I try to display graphs, for example the output of the ramp generator. But I can't get valid results. I guess it's due to some wrong properties in the graph window itself.

It should look like a sawtooth signal. But it's something weird.... I tried to play around with the settings, but I can't get value results. Datalog values should be int16 values.

I'm not sure whether I understood the functions of the settings correctly. But with the settings on the screenshot I would say that I transmit the last 50 samples (acq buffer size) every 1sec (sampling freq) and display 200 values (displ buffer) which would equal 4 seconds.

Can somebody help me in this?

Thanks!

  • Hi Phillip,

    Did you check the same on DSO ?

    Regards,

    Gautam

  • Hi Gautam,

    I'm using the TMSDOCK. So there are no DACs where I can connect an oscilloscope to. But I'm sure that the output of the ramp generator is correct because my rotor is spinning nicely. I just wanted to view some internal variables with the datalogger function and tried the ramp generator output as a test since I've never used this function before.

    Philipp

  • Phillip, so what I feel is the updation rate of the values for generating sawtooth wave and the updation rate of values in the graph are asynchronized. Hence, you're getting graph in a haphazard manner.

     Regards,

    Gautam

  • Hi,

    the datalog values are written periodically within the main ISR every 100 µs. So when I read 1000 values at low ramp frequencies (eg 15Hz) I should see more than one fully sawtooth period.

    Or maybe I still didn't got it.... :/

    Philipp