I am working with the HVPM Sensorless example in control suite using the 28335 EZDSP and my own inverter hardware. I am trying to look at various signals in the Dual Time graph. It is not working. Whne I follow the example in the documentation using start adress A= DLOG_4CH_buff1 and start address B= DLOG_4CH_buff2, I get signals that look like the signals in the documentation. When I try to view other signals such as start adress A = svgen_dq1.Ta and start address B = svgen_dq1.Tb, I get a DC line at zero for each graph. What am I doing wrong?
Thanks,
Brad Mularcik