Other Parts Discussed in Thread: TMS320F28069, CONTROLSUITE
Hello,
I want boot loader functionality in Project . I am using TMS320F28069 controller.
I have programmed the boot loader code which is available on control suite through JTAG. When I run the code , Device Manager shows USB connected in DFU mode. Then I have run the dfuprog.exe(which is available on control suite) through command prompt with the option –e to show the list of DFU device connected to PC but dfuprog.exe gives the error says that the DFU device is not connected.
1) Is there any settings required to do in dfuprog Project or in boot loader code ?
2) Is there is any procedure documents for how to use dfuprog.exe along with boot loader code?
Thanks in advance.