Other Parts Discussed in Thread: DRV8312
Hello,
I tried to run a very slow motor with InstaSPIN control. But there are some restrictions with the parameters in user.h and I get errors from USER_getErrorCode(&gUserParams) function.
The motor is a 125V 0.42A 13Hz pm motor with 4 pole pairs.
Should I change some numbers in user.h which have 'do not change' comment? Or is there any workaround?
Thank you!