This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

multiple fir 16 module usage on f28027 Piccolo

Hi everyone. I'm using fir16 module on sprc082 library downloaded from this site. I don't understand if I have to create, in order to filter with the same coefficients two differents variables, two different memory sectors for these variables. More specifically, could  I create a memory section for any of FIR16 type variables and so for relative delay buffers? The only well-working solution I've found is the following:

 

FIR16 lpf=FIR16_DEFAULTS;   
FIR16 lpf1=FIR16_DEFAULTS;
#pragma DATA_SECTION(fir,"firfilt");
FIR16 fir=FIR16_DEFAULTS;
#pragma DATA_SECTION(dbuffer,"firldb");
long dbuffer[(FIR_ORDER+2)/2];
#pragma DATA_SECTION(dbuffer1,"firldb1");
long dbuffer1[(FIR_ORDER+2)/2];
const long coeff[(FIR_ORDER+2)/2]=FIR16_LPF50_CUSTOM;

void filterInit()
{

   lpf.dbuffer_ptr=dbuffer;
   lpf.coeff_ptr=(long*)coeff;  //same coefficients for both variables
   lpf.order=FIR_ORDER;
   lpf.init(&lpf);

   lpf1.dbuffer_ptr=dbuffer1;
   lpf1.coeff_ptr=(long*)coeff; //same coefficients for both variables
   lpf1.order=FIR_ORDER;
   lpf1.init(&lpf1);

}

If this solution is correct, what is the role of the variable fir? Thank you!