Other Parts Discussed in Thread: TMS320F28335
I am using the TMS320F28335 Delfino Experimental kit. I am facing few
problems running the code from the flash.
In my code for the 3-phase system, I have multiple arrays, I have
combined the RAM sections to accommodate them. I have also increased
the stack size to 0x380.
RAML4L6 : origin = 0x00C000, length = 0x003000
I required to add 5 more array each of size 200 but faced the following problem.
Code running from RAM, less array, code work fine.
Code running from Flash, less arrays, code works fine
Code running from RAM, more arrays, "Program will not fit into memory"
Code running from Flash, more arrays, ILLEGAL ISR.
After step wise execution, it was observed that when the control exits a function with a float32 calculation, it goes into ITRAP0 and then into ILLEGAL ISR.
I commented that float32 function then the code executes fine until it encounters another float32 calculation. I have concluded that the problem has something to do with memory as the code works fine with less arrays with the same float32 functions.
In the project setting the fpu32 support is also added.
I have later used only "float" instead of "float32", still I am having the same problem.
Find attached the .cmd file (renamed to .txt) used for memory mapping.
Any help will be appreciated.
Thank you for you time.
Best Regards,
Pankaj Kadam
/*
//###########################################################################
//
// FILE: F28335.cmd
//
// TITLE: Linker Command File For F28335 Device
//
//###########################################################################
// $TI Release: 2833x/2823x Header Files and Peripheral Examples V133 $
// $Release Date: June 8, 2012 $
//###########################################################################
*/
/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in <base>\DSP2833x_Headers\cmd
//
// For BIOS applications add: DSP2833x_Headers_BIOS.cmd
// For nonBIOS applications add: DSP2833x_Headers_nonBIOS.cmd
========================================================= */
/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map */
/* Uncomment this line to include file only for non-BIOS applications */
/* -l DSP2833x_Headers_nonBIOS.cmd */
/* Uncomment this line to include file only for BIOS applications */
/* -l DSP2833x_Headers_BIOS.cmd */
/* 2) In your project add the path to <base>\DSP2833x_headers\cmd to the
library search path under project->build options, linker tab,
library search path (-i).
/*========================================================= */
/* Define the memory block start/length for the F28335
PAGE 0 will be used to organize program sections
PAGE 1 will be used to organize data sections
Notes:
Memory blocks on F28335 are uniform (ie same
physical memory) in both PAGE 0 and PAGE 1.
That is the same memory region should not be
defined for both PAGE 0 and PAGE 1.
Doing so will result in corruption of program
and/or data.
L0/L1/L2 and L3 memory blocks are mirrored - that is
they can be accessed in high memory or low memory.
For simplicity only one instance is used in this
linker file.
Contiguous SARAM memory blocks can be combined
if required to create a larger memory block.
*/
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
ZONE0 : origin = 0x004000, length = 0x001000 /* XINTF zone 0 */
RAML0L3 : origin = 0x008000, length = 0x004000 /* on-chip RAM block L0 */
//RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */
//RAML2 : origin = 0x00A000, length = 0x001000 /* on-chip RAM block L2 */
//RAML3 : origin = 0x00B000, length = 0x001000 /* on-chip RAM block L3 */
ZONE6 : origin = 0x0100000, length = 0x100000 /* XINTF zone 6 */
ZONE7A : origin = 0x0200000, length = 0x00FC00 /* XINTF zone 7 - program space */
FLASHH : origin = 0x300000, length = 0x008000 /* on-chip FLASH */
FLASHG : origin = 0x308000, length = 0x008000 /* on-chip FLASH */
FLASHF : origin = 0x310000, length = 0x008000 /* on-chip FLASH */
FLASHE : origin = 0x318000, length = 0x008000 /* on-chip FLASH */
FLASHD : origin = 0x320000, length = 0x008000 /* on-chip FLASH */
FLASHC : origin = 0x328000, length = 0x008000 /* on-chip FLASH */
FLASHA : origin = 0x338000, length = 0x007F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x33FF80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x33FFF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL : origin = 0x33FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
OTP : origin = 0x380400, length = 0x000400 /* on-chip OTP */
ADC_CAL : origin = 0x380080, length = 0x000009 /* ADC_cal function in Reserved memory */
IQTABLES : origin = 0x3FE000, length = 0x000b50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008c /* IQ Math Tables in Boot ROM */
FPUTABLES : origin = 0x3FEBDC, length = 0x0006A0 /* FPU Tables in Boot ROM */
ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML4L6 : origin = 0x00C000, length = 0x003000 /* on-chip RAM block L1 */
//RAML5 : origin = 0x00D000, length = 0x001000 /* on-chip RAM block L1 */
// RAML6 : origin = 0x00E000, length = 0x001000 /* on-chip RAM block L1 */
RAML7 : origin = 0x00F000, length = 0x001000 /* on-chip RAM block L1 */
ZONE7B : origin = 0x20FC00, length = 0x000400 /* XINTF zone 7 - data space */
FLASHB : origin = 0x330000, length = 0x008000 /* on-chip FLASH */
}
/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : > FLASHA PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0L3,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : > RAML4L6 PAGE = 1
.esysmem : > RAMM1 PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHC PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
/* Allocate DMA-accessible RAM sections: */
DMARAML4 : > RAML4L6, PAGE = 1
DMARAML5 : > RAML4L6, PAGE = 1
DMARAML6 : > RAML4L6, PAGE = 1
DMARAML7 : > RAML7, PAGE = 1
/* Allocate 0x400 of XINTF Zone 7 to storing data */
ZONE7DATA : > ZONE7B, PAGE = 1
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
/* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
.adc_cal : load = ADC_CAL, PAGE = 0, TYPE = NOLOAD
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/