Other Parts Discussed in Thread: CCSTUDIO, MOTORWARE, DRV8301, BOOSTXL-DRV8301
Following the instructions as per the quick start guide, when running the InstaSpin_FOC GUI, the follow error message appeared:
"Restarting Program Model...
Initializing target : C:\ti\guicomposer\webapps\InstaSPIN_FOC_F2806xM\appConfig.ccxml
Connecting target: Texas Instruments XDS100v2 USB Emulator_0/C28xx
sun.org.mozilla.javascript.internal.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error connecting to the target: emulation failure occurred (<Unknown source>#14) in <Unknown source> at line number 14Restart Completed."
Here is what I have verified thus far:
- installed GUI composer InstaSpin on PC
- installed motorware and code composer studio 5.4 (from disk)
- connected board to 15V dc power supply (PVDD pin connected to positive of the power supply and GND pin connected to the ground of the power supply)
- control card is clamped tightly to the board and connected to PC via USB cable at J01
- position of switches on the control card are verified: controlCARD SW1-SW3: UP-UP, Down-Down, UP-UP
- Power LED on the control card is green
- checked device manager for USB ports:"TI XDS100 Channel A" and "TI XDS100Channel B"; under ports I can see USB Serial Port (COM6)
- 3 phase BLDC motor is connected to the corresponding ports on the board
In addition, when running the debug from lab 1, the following error message is generated:
Error connecting to the target:
(Error -1135 @ 0x0)
The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation.
(Emulation package 5.1.73.0)
Could you please suggest a solution?
Thanks for the help.