Other Parts Discussed in Thread: TMS320F28335
hii, I am using TMS320F28335 DSP Board with JTAG emulator (XDS100v2) (connected through USB to the Laptop). I am using this to generate PWM signal which is fed to the gate driver of an inverter. Whenever I am running this, at the beginning with lower DC input voltage it is working fine and when I am increasing DC input voltage of the inverter little bit more it is showing the following error
C28xx: Error: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 5.1.73.0)
After sometime it is turning OFF automatically.
Again when I am starting it from the beginning it working fine with lower Input DC voltage and after some higher DC input voltage it is showing the same error.
Please help me in this regard.