Hi,
I am learning the C2000 DSC with the F28069 and working on the SCI module these days.
I used the RX/TX FIFO and the RX FIFO worked well but I had some difficulty in using the TX FIFO.
I set the FIFO level of RX/TX both 2 and I want to send two chars to the DSC and then it will sent the same chars back.
I notice that the TX interrupt should be disabled if there is nothing to send or the interrupt will occur all the time. So I just disable the TX interrupt in the TX ISR.
But every time I send two chars to the DSC, it will send the same chars back TWICE.
For example, I send "Hi" to the DSC and it will send "HiHi" back.
The initialization codes are shown below.
// Test 1,SCIA DLB, 8-bit word, baud rate 0x0103, default, 1 STOP bit, no parity void scia_echoback_init() { // Note: Clocks were turned on to the SCIA peripheral // in the InitSysCtrl() function SciaRegs.SCICCR.bit.STOPBITS = 0; // 1 stop bit SciaRegs.SCICCR.bit.PARITY = 0; // Odd parity SciaRegs.SCICCR.bit.PARITYENA = 0; // No parity SciaRegs.SCICCR.bit.LOOPBKENA = 0; //No loopback SciaRegs.SCICCR.bit.ADDRIDLE_MODE = 0; //Idle-line mode SciaRegs.SCICCR.bit.SCICHAR = 7; //8 char bits SciaRegs.SCICTL1.bit.RXERRINTENA = 0; // Disable RX ERR SciaRegs.SCICTL1.bit.SWRESET = 0; // SCI software reset SciaRegs.SCICTL1.bit.TXWAKE = 0; // Disable TXWAKE SciaRegs.SCICTL1.bit.SLEEP = 0; // Disable SLEEP SciaRegs.SCICTL1.bit.TXENA = 1; // Transmitter enabled SciaRegs.SCICTL1.bit.RXENA = 1; // Receiver enabled SciaRegs.SCICTL2.bit.TXINTENA =1; // Enable TXRDY interrupt SciaRegs.SCICTL2.bit.RXBKINTENA =1; // Enable RXRDY/BRKDT interrupt SciaRegs.SCIHBAUD =0x0001; // 9600 baud @LSPCLK = 22.5MHz (90 MHz SYSCLK). SciaRegs.SCILBAUD =0x0024; // 22500000/(9600*8)-1=291.968 } // Initalize the SCI FIFO void scia_fifo_init() { // SCIFFTX SciaRegs.SCIFFTX.bit.SCIRST = 1; // resume transmit or receive SciaRegs.SCIFFTX.bit.SCIFFENA = 1; // Enable SCI FIFO SciaRegs.SCIFFTX.bit.TXFIFOXRESET = 1; // Re-enable transmit FIFO operation SciaRegs.SCIFFTX.bit.TXFFINTCLR = 1; // Clear TXFFINT flag //SciaRegs.SCIFFTX.bit.TXFFIENA = 1; // TX FIFO interrupt based on TXFFIVL match is enabled SciaRegs.SCIFFTX.bit.TXFFIL = FifoLevel; // Transmit FIFO interrupt level // SCIFFRX SciaRegs.SCIFFRX.bit.RXFFOVRCLR = 1; // Clear RXFFOVF flag SciaRegs.SCIFFRX.bit.RXFIFORESET = 1; // Re-enable receive FIFO operation SciaRegs.SCIFFRX.bit.RXFFINTCLR = 1; // Clear RXFFINT flag SciaRegs.SCIFFRX.bit.RXFFIENA = 1; // RX FIFO interrupt based on RXFFIVL match is disabled SciaRegs.SCIFFRX.bit.RXFFIL = FifoLevel; // Receive FIFO interrupt level // SCIFFCT SciaRegs.SCIFFCT.bit.CDC = 0; // Disables auto-baud alignment SciaRegs.SCIFFCT.bit.FFTXDLY = 0; // FIFO transfer delay SciaRegs.SCICTL1.bit.SWRESET = 1; // Relinquish SCI from Reset SciaRegs.SCIFFTX.bit.TXFIFOXRESET=1; SciaRegs.SCIFFRX.bit.RXFIFORESET=1; }
The RX ISR.
interrupt void sciaRxFifoIsr(void) { uint16 i = 0; RxIsrCount++; for (i = 0;i < FifoLevel;i++) { RxData[i] = SciaRegs.SCIRXBUF.all; } SciaRegs.SCIFFTX.bit.TXFFIENA = 1; // TX FIFO interrupt based on TXFFIVL match is enabled SciaRegs.SCIFFRX.bit.RXFFOVRCLR = 1; // Clear Overflow flag SciaRegs.SCIFFRX.bit.RXFFINTCLR = 1; // Clear Interrupt flag PieCtrlRegs.PIEACK.all |= M_INT9; // Issue PIE ack }
The TX ISR.
interrupt void sciaTxFifoIsr(void) { TxIsrCount++; uint16 j = 0; for (j = 0;j < FifoLevel;j++) { SciaRegs.SCITXBUF = RxData[j]; } SciaRegs.SCIFFTX.bit.TXFFINTCLR = 1; // Clear SCI Interrupt flag SciaRegs.SCIFFTX.bit.TXFFIENA = 0; // TX FIFO interrupt based on TXFFIVL match is disabled PieCtrlRegs.PIEACK.all |= M_INT9; // Issue PIE ACK }
And I find that if I change the order of clearance the SCI Interrupt flag and the TX FIFO interrupt enable bit in the TX ISR as shown below, the DSC will work well and just send me the correct chars.
interrupt void sciaTxFifoIsr(void) {
TxIsrCount++; uint16 j = 0; for (j = 0;j < FifoLevel;j++) { SciaRegs.SCITXBUF = RxData[j]; } SciaRegs.SCIFFTX.bit.TXFFIENA = 0; // TX FIFO interrupt based on TXFFIVL match is disabled SciaRegs.SCIFFTX.bit.TXFFINTCLR = 1; // Clear SCI Interrupt flag PieCtrlRegs.PIEACK.all |= M_INT9; // Issue PIE ACK }
I really don't know why.
I put my whole project as the attachment.
I am looking forward for your help.
:)
thanks and regards
Di