This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi -
I'm evaluating InstaSPIN control to replace existing motor control in our products. I have one axis that screeches when I do a long move in one direction and is quiet when I move it in the opposite direction. The videos are attached.
I've changed bandwidth and all bandwidths settings when it successfully runs exhibit the noise. I've played with acceleration and jerk and still get noisy moves in the one direction. If I lower the velocity significantly, the noise goes away. I get the noise with both ST and S-curve profiles.
This motor uses an off-axis linear encoder. The actual number of encoder counts per motor revolution is fractional (6502.4 counts). The qep is set up with (4*1626 -1) counts which is 6503. Could this be the source of the noise in one direction?
The position error on the noisy move looks good compared to our current motor control, but the screeching is a problem.
Thanks-
Mary