This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have created a workspace and imported several labs into the project workspace. However, when I copy and paste a file within a project such "Copy of proj_lab01.c", I cannot find where this file is located. It seems to be, maybe, some sort of referenced file.
Kurt Kloesel
Hi Kurt,
When you copy and paste a file in a project, it will be placed in your folder where the project located. In case you import project without selecting the checks as the following figure:
then your project is sill in where you browsed to.
In case you selected "cope projects into workspace" then the folder of the imported project will be in the same folder where you place the workspace of CCS.
That's all,
Tran
Hi Kurt,
You make a good observation. You are right, the small arrow indicates that the file is being referenced by the CCS project instead working on another copy of the file. This is convenient when you want a single copy of your work and may have multiple projects referencing it. Your choice. A complete description of CCS options like this can be found here: .
You can look at a files properties by right-mouse-clicking on that file and select "properties". In the window that opens note the Resource section and then note the location of the file. In the screen capture below you see that adc.c from MotorWare is referenced or linked by proj_lab02a with a base reference of where the MW installation directory is located. You can this is fully in the "Resolved location" section.
It is really your choice whether to copy or link the file into your project.
Jeff
Did a reply answer your question? If yes, please click the "Verify Answer" button located at the bottom of that post. |
||
InstaSPIN-FOC/MOTION User's Guide |
OK, that procedure works. Not exactly what I expected, but workable.
When I used the copy procedure on the referenced file. I found that altering one file would change the other one. Example:
"proj_1.c" (referenced) copied to "Copy of proj_1.c" (also referenced). Any changes to "Copy of proj_1.c" would show up in "proj_1.c". It was late at night when I discovered this, I was really confused.
Thanks for your help.
Kurt