Other Parts Discussed in Thread: LAUNCHXL-F28069M
Hello -
I am currently evaluating InstaSPIN-MOTION for a custom actuator we are building. I am currently using LAUNCHXL-F28069M + BOOSTXL-DRV8305 Hardware and a BLDC motor rated at 360kv (24V).
I have a 4096 cpr magnetic encoder attached to the motor, and attached to the LaunchPad (QEP_A port).
When I run Inertia ID using Lab 5c (sensorless), I am able to get inertia and friction measurements up to the rated 8krpm (I should probably state that there is currently no load on the motor).
However, when running Lab 12a (sensored), I get measurements fine up to about 5.5krpm. Anything higher than that gives Error 2003. However, no matter what value I put into VelIdTorqueRampTime_sec, I still get error 2003. I have tried reconfiguring the encoder for 2048 cpr and 1024 cpr as well with no luck (thinking that maybe that speed was too much for the encoder/QEP port).
Please advise what to look for here.
Lastly, when I use lab 12b to test the velocity controller (using inertia and friction from a valid test ~5krpm) the motor makes unpleasant noise and goes crazy if i try to exceed a certain speed (4krp or higher). I assume this is related to the same issue above?
Any insight is much appreciated!
Best,
asifjahmed