Hello,
I am using DRV8312 with F28069 ControlCard, the GUI control works fine, i am able to control the motor with only GUI.
Now i wanted to test the lab examples given in the "motorware" - C:\ti\motorware\motorware_1_01_00_15\sw\solutions\instaspin_foc\boards\drv8312kit_revD\f28x\f2806xF\projects\ccs5\proj_lab03b
Tested target configuration - OK Successful
Build - OK
Debug - OK
In the debug when i RUN the code - RED LED 2 in contolCard blinks but no response by the motor!!!
1) what is my mistakes?
2) what is the jumper settings to run the lab examples given?
3) I checked where the code gets in to infinite loop, here is the statement in line 333
for(;;)
{
// Waiting for enable system flag to be set
while(!(gMotorVars.Flag_enableSys));
the control gets in to this infinite loop.
Please help me come out of this problem..
Regards
Shashanka