This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Anyone please tell what should i do ......
**** Build of configuration Debug for project bldc3_1_281x_CCS3x ****
"C:\\TI 6\\ccsv6\\utils\\bin\\gmake" -k all
'Building target: ../bldc3_1.out'
'Invoking: C2000 Linker'
"C:/TI 6/ccsv6/tools/compiler/ti-cgt-c2000_6.4.2/bin/cl2000" -v28 -ml -g --define="_DEBUG" --define="LARGE_MODEL" --define="TARGET_IS_F2812" --quiet --display_error_number --diag_wrap=off --obj_directory="C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj" -z -m"../bldc3_1.map" --stack_size=0x50 --warn_sections -i"C:/TI 6/ccsv6/tools/compiler/ti-cgt-c2000_6.4.2/lib" -i"C:/TI 6/ccsv6/tools/compiler/ti-cgt-c2000_6.4.2/include" -i"D:/Trial CodeComposer/bldc3_1_281x_CCS3x" -i"C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/build" -i"c:/CCStudio_v3.1/c2000/cgtools/lib" --reread_libs --display_error_number --diag_wrap=off --xml_link_info="bldc3_1_281x_CCS3x_linkInfo.xml" --rom_model -o "../bldc3_1.out" "C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/DSP281x_CodeStartBranch.obj" "C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/DSP281x_DefaultIsr.obj" "C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/DSP281x_GlobalVariableDefs.obj" "C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/DSP281x_PieCtrl.obj" "C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/DSP281x_PieVect.obj" "C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/DSP281x_SysCtrl.obj" "C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj" "C:/tidcs/c28/DSP281x/v100/DSP281x_headers/cmd/DSP281x_Headers_nonBIOS.cmd" "../F2812_EzDSP_RAM_lnk.cmd" "C:/tidcs/DMC/c28/v32x/lib/dmclib/cIQmath/lib/IQmath.lib" -l"rts2800_ml.lib"
undefined first referenced
symbol in file
>> Compilation failure
--------- ----------------
_DLOG_4CH_init C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_DLOG_4CH_update C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_F281X_EV1_BLDC_PWM_Init C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_F281X_EV1_BLDC_PWM_Update C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_F281X_EV1_DRIVE_Init C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_F281X_EV1_DRIVE_Update C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_F281X_EV1_HALL3_Init C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_F281X_EV1_HALL3_Read C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_F281X_adc04u_drv_init C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_F281X_adc04u_drv_read C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_mod6cnt_calc C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_pid_reg3_calc C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_rmp2_cntl_calc C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_rmp_cntl_calc C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
_speed_prd_calc C:/tidcs/DMC/c28/v32x/sys/BLDC3_1_281x/cIQmath/obj/bldc3_1.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "../bldc3_1.out" not built
gmake: *** [../bldc3_1.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****