Hi,
We are using F28377D with docking station for multilevel converter. We need to convert large number of analog signals and configured the ADC-A, ADC-B, ADC-C,ADC-D with SOC0 and SOC1. The results of the ADCs are not correct particularly when the input signal is on higher side. The TI example code adc_soc_epwm gives accurate results with single conversion (with only SOC0). However, when we modified the SetupADCEpwm() function as below, the ADC results are not correct. In the modified code, we initiate the trigger after the end of SOC1 conversion instead of end of SOC0 conversion. For the testing, we connected the DACA (pin 9) output to the ADC-A2 input (15) externally and modified the DACA data register from code. For this we made the channel select for ADC-A from A0 (as in example ) to A2.
Altogether we need to convert 14 signals at the sampling rate of 20000 Hz.. What is the suggested configuration for this?
void SetupADCEpwm(Uint16 channel)
{
Uint16 acqps;
//determine minimum acquisition window (in SYSCLKS) based on resolution
if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION){
acqps = 14; //75ns
}
else { //resolution is 16-bit
acqps = 63; //320ns
}
//Select the channels to convert and end of conversion flag
EALLOW;
AdcaRegs.ADCSOC0CTL.bit.CHSEL = channel; //SOC0 will convert pin A0
AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is 100 SYSCLK cycles
AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
//Added lines for the second input
AdcaRegs.ADCSOC1CTL.bit.CHSEL = 3; //SOC0 will convert pin A0
AdcaRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is 100 SYSCLK cycles
AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
//Modified to trigger the event at the end of SOC1 instead of SOC0
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
}
We also looked at the suggestion at https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/349011 but could not resolve the problem.
-Shambhu