This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My configuration Hardware:
- TMS320F28335 Experimenter Kit
I have a problem with the McBSP used as SPI operation as Master.
When i send 2 words (more than 1 word), the first word has the good number of clock (16 clocks for 16 bits) but the second word has 18 clocks for only 16 valid bits as seen on figure below.
My configuration software:
/* Step 1 : Place the transmitter and receiver inreset */
OMCB_McbspaRegs.SPCR2.bit.XRST = 0; /* Transmitter reset */
OMCB_McbspaRegs.SPCR1.bit.RRST = 0; /* Receiver reset */
/* Step 2 : Place the sample rate generator in reset */
OMCB_McbspaRegs.SPCR2.bit.GRST = 0; /* Sample Rate generator Reset */
OMCB_McbspaRegs.SPCR2.bit.FRST = 0; /* Frame Sync generator reset */
/* Step 3 : Program registers that affect SPI operation */
/* Serial Port Control 1 Register */
OMCB_McbspaRegs.SPCR1.bit.DLB = 0; /* For Test only */
OMCB_McbspaRegs.SPCR1.bit.CLKSTP = 2; /* Low active state without delay, with CLKXP = 0 and CLKRP = 0 */
/* The McBSP transmits data on the rising edge of CLKG */
/* and receives data on the falling edge of CLKG */
/* Serial Port Control 2 Register */
/* Receive Control Register 1 */
OMCB_McbspaRegs.RCR1.bit.RWDLEN1 = 2; /* 16-bits word (receiver) */
OMCB_McbspaRegs.RCR1.bit.RFRLEN1 = 0; /* 1 word length (receiver) */
/* Receive Control Register 2 */
OMCB_McbspaRegs.RCR2.bit.RDATDLY = 1; /* This setting provides the correct setup time on the FSX Signal */
OMCB_McbspaRegs.RCR2.bit.RWDLEN2 = 2; /* 16-bits word */
OMCB_McbspaRegs.RCR2.bit.RFIG = 0; /* Frame synchronisation detect */
/* Transmit Control Registers 1 */
OMCB_McbspaRegs.XCR1.bit.XWDLEN1 = 2; /* 16-bits word (transmitter) */
OMCB_McbspaRegs.XCR1.bit.XFRLEN1 = 0; /* 1 words length (transmitter) */
/* Transmit Control Registers 2 */
OMCB_McbspaRegs.XCR2.bit.XWDLEN2 = 2; /* 16-bits word */
OMCB_McbspaRegs.XCR2.bit.XDATDLY = 1; /* This setting provides the correct setup time on the FSX Signal */
OMCB_McbspaRegs.XCR2.bit.XFIG = 0; /* Frame synchronisation detect */
/* Sample Rate Generator 1 Register */
OMCB_McbspaRegs.SRGR1.bit.CLKGDV = 3; /* clock = Input clock / (CLKGDV+1) => clk=> 37.5/4 = 9.375Mhz */
OMCB_McbspaRegs.SRGR1.bit.FWID = 0; /* Frame Width = 0 => 1 Pulse */
/* Sample Rate Generator 2 Register */
OMCB_McbspaRegs.SRGR2.bit.CLKSM = 1; /* CLKSM = 1 and SCLKME= 0 => Input clock (LSPCLK) */
/* Pin Control Register */
OMCB_McbspaRegs.PCR.bit.FSXM = 1; /* Transmit frame synchronization is generated internally by the Sample Rate generator */
OMCB_McbspaRegs.PCR.bit.FSRM = 1; /* Receive frame synchronization is supplied by the sample rate generator */
OMCB_McbspaRegs.PCR.bit.CLKXM = 1; /* In clock stop mode => The McBSP is a master in the SPI Protocol */
OMCB_McbspaRegs.PCR.bit.CLKRM = 1; /* digital loopback disable => */
/* Internal MCLKR is driven by the sample rate generator of the McBSP */
OMCB_McbspaRegs.PCR.bit.SCLKME = 0; /* CLKSM = 1 and SCLKME= 0 => Input clock (LSPCLK) */
OMCB_McbspaRegs.PCR.bit.FSXP = 1; /* Transmit frame-synchronization pulses are active low */
OMCB_McbspaRegs.PCR.bit.CLKRP = 0; /* The McBSP receives data on the falling edge of CLKG */
OMCB_McbspaRegs.PCR.bit.CLKXP = 0; /* The McBSP transmits data on the rising edge of CLKG */
/* McBSP Interrupt Enable Register */
OMCB_McbspaRegs.MFFINT.bit.XINT = 1; /* Enable Transmit Interrupts */
OMCB_McbspaRegs.MFFINT.bit.RINT = 1; /* Enable Receive Interrupts */
/* Step 4 : Enable the sample rate generator */
OMCB_McbspaRegs.SPCR2.bit.GRST = 1; /* Enable the sample rate generator */
for(cpt = 0; cpt < 200; cpt++); /* Wait at least 2 SRG clock cycles */
/* Step 5 : Enable the transmitter and receiver */
OMCB_McbspaRegs.SPCR2.bit.XRST=1;
OMCB_McbspaRegs.SPCR1.bit.RRST=1;
/* Step 6 : Enable the Frame synchronization logic of the sample rate generator */
OMCB_McbspaRegs.SPCR2.bit.FRST=1;
I use interrupt for Tx and Rx.
When the McBSP work on Loopback, they read the correct value.
But when i want communicate with other device, the 'useless' clocks cause a bad reading word.
Thanks for helping
Guillaume,
If you take the existing mcbsp example, do you see the same issue?
Can you share the mcbsp functional code? I would like to see if i can duplicate this on the bench.
Thanks,
Mark
Hi Mark,
By default the example provide by TI don't work as SPI operation.
But i have initialize the McBSP as defined in Application note.
I have zip my code for McBSP protocol.
Thanks for helping16_01_19_Ti_exemple.7z
Guillaume,
There is an example in controlSUITE for McBSP in SPI loopback mode. It should be located at ..\controlSUITE\device_support\f2833x\v141\DSP2833x_examples_ccsv5\mcbsp_spi_loopback.
Can you share which application note you are referring to? Do you mean the User Guide?
I will see if I can reproduce this issue with your code and let you know.
-Mark
Hi,
In Ti example, a clock is missing before the 1 words (word 1 = 16 bit, word 2 = 15 bit, etc...)
i'm looking this problem on the forum.
I hase use this tutorial:
Hi,
After verification,
In the TI example, only 1 word is sent (OMCB_McbspaRegs.XCR1.bit.XFRLEN1 = 0 and OMCB_McbspaRegs.RCR1.bit.RFRLEN1 =0)
I have modified the number of bit by word (OMCB_McbspaRegs.RCR1.bit.RWDLEN1 and OMCB_McbspaRegs.XCR1.bit.XWDLEN1 to 2 ) in order to send 16 bits.
So if I modify this bit to 1 in order to send 2 (same) words.
The McBSP sends the last word written in the buffer twice.
- First word with 16 bits and second word with 15 bits (15 clock cycles).
---------------------------------------------
if I want to send 2 different words I have two choices:
- either :
OMCB_McbspaRegs.DXR1.all = 0xAAAA;
while(OMCB_McbspaRegs.SPCR2.bit.XRDY == 0){} // wait empty Tx buffer
OMCB_McbspaRegs.DXR1.all = 0x9999;
- or by interruption
with MCB_McbspaRegs.MFFINT.bit.XINT = 1 and OMCB_McbspaRegs.MFFINT.bit.RINT = 1
and write a new word in OMCB_McbspaRegs.DXR1.all during the treatment of the interruption
In this case, i see the first word with 16 bits and the second word with 18 bits (18 clock cycles).
The first 2 clock cycles aren't expected.
after this 2 clock cycles i see my word 0x9999.