Hello,
I am using a TI PLC Development kit based on the F28PLC83 chip (firmware 7.7.1.6). I compile and play with the HostApplication, which runs nice. However, I would like to go beyond what this application currently enables me to do. Especially, I would like to use my G3 board as a sniffer to monitor in real time the G3 traffic that goes on the PLC link even if not sent from / to my G3 board.
Is it something possible? If yes, how should I configure the board? Maybe some special parameters to pass upon initialization, maybe in the G3_ServiceNodeManagement::StartProcess()?...
I would gladly welcome any help, even the tiniest, because I am stuck here since days :) !
Thanks a lot in advance, and best regards,
Alexis