This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
thank you for providing the motorware solutions.
I'm trying to run the two motor examples and it works fine in speed control mode (lab12c). Now i would try something with a torque controller. I've read that the speed controller is only a higher controller for the included torque controller.
Is there an easy way to change the speed controller form lab12c to a torque controller?
I use the two motors to eliminate the gear backlash. For breaking i will run booth motors at the same gear and one of them with an inverse torque to the other. For rotating i will only change the ratio of torque. I hope that when both motor have set the same torque but different directions that they don't move.
Thanks in advance.