This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am having trouble with the connection of my ADC and F28377S launchpad by UPP, any schematic or circuit diagram would be very helpful.
Hi Tejas,
We don't have custom board schematic for uPP interface. The IO interface for UPP is very straight forward. It has dedicated TX and RX pins and CLK which is output in TX mode and input in RX mode. There are three control signal ENABLE and START and WAIT. Polarity of these signals are configurable and if any of these are not supported from external device then can be configured to ignore. Please refer section "24.4 IO Interface and System Requirements" to understand the interface. All signals are connected point-to-point to external device.
If you have some specific question about connecting any signal, please let us know.
Regards,
Vivek Singh