Other Parts Discussed in Thread: CONTROLSUITE, TMDSCNCD28335
Hello everyone,
I am digitally controlling a power converter for which I am going to use the control card (TMDSCNCD28335). My requirements for the DSP are most certainly only the JTAG interface, the PWM peripheral, and the ADC peripheral. I am currently designing the PCB of my converter and implement the footprint for the DIMM100 board. Following the schematic in the controlSUITE, I have three questions:
1. What exactly are the 3V3_ISO, RX-ISO and TX-ISO (on the DIMM-100 connector, pin1, pin 2, pin 51 and pin 52) used for? Same applies for the isolated GND. Are any of these necessary or only if a certain peripheral is used?
2. Related to question 1, the digital isolator (component U4A) has SCI-TX and SCI-RX. What are their purpose?
3. To my understanding, all I need to be aware of is to ensure a 5V supply for the control card (which is on the controlCARD itself converted to the necessary voltage levels for the DSP), the JTAG connections TDI, TDO, TRSTn, EMU0, TCK, TMS, EMU1 for programming purposes as well as the pins for my EPWM and ADC peripherals. Is that correct or am I missing anything crucial?
Hope to hear from you. Thank you.
BR,