This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Apologize if the question is related to very old environments. Seeking some understanding:
When I build our code with CCS 3.3 for F812, the intel hex file shows that at address 0x3f77f6 a longword value is generated. As I change the code, this value also changes. I am guessing this is a checksum or CRC of the code. If so what is the algorithm used? Is the implementation available in the library?
If not what is this value?
Todd
That is perfect. Thanks. I slowly was going to that conclusion but this gives the reference.
Thanks, srini