Hi,
I could successfully use the F28035 PMSM code for driving the BLDC motor with drv8301 experimental kit. I would desire to run the BLDC motor as a generator with the same drive. Is there any way.
thx
KVRao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I could successfully use the F28035 PMSM code for driving the BLDC motor with drv8301 experimental kit. I would desire to run the BLDC motor as a generator with the same drive. Is there any way.
thx
KVRao
My understanding is: when the BLDC runs as a generator, the output voltage will be rectified by the freewheel diodes embedded in the inverter, without any control applied. With a control of the BLDC motor as generator, are you still trying to do rectifier job or some other functions?
Hi evs, Thanks for your inputs. Actually I intend to use a battery for source and sinking should be possible too. Making a toque controller is sensible. Could you please suggest how to do this. Maybe if I get the opportunity I could try it once.
Thx
KVRao
I think a saver way is to use a bench power supply with a resistor load in parallel. To get thing working.
After that. use a battery with a fuse and a serial resistor. So that the generator current controller has some resistance to control against and not directly into a voltage source. If that works correctly lower the serial resistor till it is 0 mohm. I think that is the hard part to get that working safely because of the speed and accuracy of the current measurement.