Hello all, I am trying to get information on the following:
#1 TMDSHVMTRINSPIN
#2 TMDSHVMTRPFCKIT
#3 TMDXHVMTRKIT5X
Q1. If I use Kit#1 (InstaSpin), can this kit support various types of control algorithm implementation such as variable frequency, field oriented, sensorless back EMF, velocity feedback control, etc? InstaSpin include C/C++ implementation and/or graphical user interface? Any example or explanation step by step on how to try motor speed control with this kit, code example or block diagram when implemented in InstaSpin are also useful. Based on product description of kit #1, I don't see this explanation.
Q2. For Kit#2, if I understand correctly this kit itself also supports the motor I selected which is 3 Phase motor. The product description does show the various types of controller support listed above. In order to implement control algorithm, the software features include controlSUITE which is different from InstaSPIN of Kit#1. Does controlSUITE support C/C++ code implementation and/or graphical user interface? What are the highlight difference between Kit#1 and #2 in terms of flexibility of c