Hi team,
On the new F28075, can someone please confirm:
-The maximum QEP clock frequency input from encoder?
-Can all 3 QEP’s operate simultaneously without any pin overlapping?
Thanks in advance,
Billy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Billy,
BillyO said:On the new F28057, can someone please confirm:
I believe you mean the F28075.
BillyO said:The maximum QEP clock frequency input from encoder?
The QEP input timing requirements are provided in the device datasheet, SPRS902C, Table 5-59.
BillyO said:Can all 3 QEP’s operate simultaneously without any pin overlapping?
Yes. Please see the pin muxing Table 4-1 in the datasheet SPRS902C, p.11.
- David