Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software: Code Composer Studio
For ADC, I have a code as follow in 'examples_setup.h'
=========================================================
#define CPU_FRQ_200MHZ 1
#define ADC_SAMPLING_FREQ 25000.0L
#define EPWM_HSPCLKDIV 1
#define EPWM1_PERIOD 2000
#define EPWM1_DUTY_CYCLE 1000
#define EPWM2_PERIOD 200000
#define EPWM2_DUTY_CYCLE 100000
=========================================================
Does ADC use EPWM1 and EPWM2 both? or just use EPWM1?
Also, In case of using sampling frequency as 26kHz,
I calculated EPWM DUTY CYCLE and PERIOD values and they are not exact integer.(ex:1290.1229)
In that case, should I use just '1290' instead of '1290.1229'?