Part Number: TMS320F28335
Hi, I am using the TMS320F28335 to read data from a AD7657 ADC using a parallel interface without much luck. The examples I've found all seem to be using SPI.
I have already configured the external zone. XINTF clock is enabled, the timing registers are set, x16 data bus selected, the appropriate XD, XA, XZCS, etc. are selected.
A pointer to the first memory location of zone 6 is used to read the data from the external zone.
A potentiometer is connected to the input of the ADC. I am viewing the contents of zone 6 using the Memory Browser in CCS. There seems to be random values populating the memory. I have command the ADC to reset so I expect zeros to be returned.
Has anyone else worked with peripherals which communicate to external zones outside of SPI that can point in the right direction?