This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M36P63C2: Program c28 and M3 using command line instead of Uniflash

Part Number: F28M36P63C2
Other Parts Discussed in Thread: UNIFLASH,

Hi,

I am trying to program the M3 core and C28 via the command line and find that only M3 gets programmed and there is no way I am able to load C28.

Is there any way I could program them together or individually using command line?

I have to program 3 of these devices and command line will make life easy.

Please help, if anyone has idea in this regard.

Thanks,

Sanjana