Other Parts Discussed in Thread: LAUNCHXL-F28027F, LAUNCHXL-F28069M, BOOSTXL-DRV8305EVM
I'm investigating a constant torque motor controller that can can maintain torque to within +/- 0.75% of setpoint over a speed range of (-20 RPM) to (300 RPM). I have three questions if I may:
- Control at low speeds from 0 RPM to ??? using FOC are augmented by the Forced Angle concept described in TI's literature. Forced Angle seems to be primarily for initial starting of a motor whose target RPM is much higher. Is it also useful for control and, if not, where is the low-end speed cutoff for using FOC with a 2-pole-pair BLDC motor?
- I cannot find anything in the literature or the LAUNCHXL-F28027F lab project software source that supports the FOC maintaining constant torque control when motor speeds become negative. The mechanical linkage on the motor's output will, in certain unusual process conditions, allow the motor to be driven "backwards". Ideally, the motor would maintain constant torque control during these episodes, will FOC accomplish that?
- If either the low-speed or the negative speed issues disqualify FOC for constant torque control, then is there an alternative technology TI offers to make this possible without going to a rotation sensor solution?
Thank you very much!
David