Part Number: TMS320F28027F
Other Parts Discussed in Thread: MOTORWARE, DRV8301, DRV8305
Hello -
I am designing custom hardware for a traction motor application. I have a few questions/concerns around startup torque.
- I know several different aspects of zero-speed startup have been discussed previously, but most of those posts are 2-3 years old, so I am just curious if there are any recent developments regarding zero-speed startup (with heavy load, a la traction motor)
- I see that Motorware 17 has been released and it contains a lab for hall effect sensor startup using BLDC commutaion, with transition to FOC. Does this work for pure torque control as well (speed controller disabled)? I honestly would love to avoid the use of the sensors if at all possible.
- Are there any examples/guidelines to using hall-effect sensors with the F28027F? IO is limited on this board after incorporating a DRV8301/DRV8305 w/ SPI, etc.
Any advice is much appreciated!
Best,
-asifjahmed