This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL-F28377S
Hi,
I have an application on LAUNCHXL-F28377S that I would like to enhance with wireless commands. I have a few questions about using LAUNCHXL-CC1310 with the F28377:
1) Is it possible to mate them and pass commands from cc1310 to F28377s? (I don't need to pass data back from F28377)
2) If so, is there an example program that shows how to do simple commands?
3) Also, is it possible for the F28377s to control when it looks for commands from cc1310? I have a tight real-time schedule, and portions of it cannot be interrupted. I actually would prefer to poll for commands at times that are convenient.
Thanks for your help!
-dave