Part Number: TMS320F28335
Hi all,
I am working on C28x F28335 Delphino micro-controller custom boards, i want to establish communication between these two similar boards through SCI interface i.e.,SCIB on one and SCIC on another.
I tried using loop back mechanism for each board separately, it is working good. While, if i remove loop back and connect these custom boards to each other, the most significant nibble on the receiving side is wrong, for example when I'm trying to transmit data (0xAA) from one board and receive the same data on other board i'm able to receive 0x5A or 0x4A instead of 0xAA (correct Data). The Frame error bit of SCIRXBUF is remaining 1 each and every time I transmit the Data. I have tried to check the transmitted data on the TX pin of microcontroller and please refer the attached file.
I have configured the SCIFFRX buffer with RXFFIL length as1 byte and RXFFIENA is enabled.
Here attached my project file.
/**********************************************************************************************************************************************************/
#if 1
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#pragma CODE_SECTION(InitFlash, "ramfuncs");
#define CPU_FREQ 150E6
#define LSPCLK_FREQ CPU_FREQ/4
#define SCI_FREQ 100E3
#define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1
// Prototype statements for functions found within this file.
//__interrupt void scicTxFifoIsr(void);
__interrupt void scicRxFifoIsr(void);
void scic_fifo_init(void);
void InitScicGpio();
Uint16 rdataB[8]; // Received data for SCI-A
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadEnd;
extern Uint16 RamfuncsRunStart;
extern Uint16 RamfuncsLoadSize;
void Delay()
{
unsigned int i,j;
for(i = 0;i < 500;i++)
for(j = 0;j < 500;j++);
}
Uint16 Recv_dat = 0x00;
void main(void)
{
Uint16 i;
unsigned char SendChar = 0x00;
InitSysCtrl();
InitScicGpio();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
InitFlash();
EALLOW;
PieVectTable.SCIRXINTC = &scicRxFifoIsr;
EDIS;
scic_fifo_init(); // Init SCI-B
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER8.bit.INTx5 = 1; // PIE Group 9, INT3
IER |= 0x080;
EINT;
while(1)
{
for(i = 0;i < 8;i++)
{
ScicRegs.SCITXBUF=0x55;//SendChar;
Delay();Delay();Delay();Delay();
Delay();Delay();Delay();Delay();
Delay();Delay();Delay();Delay();
SendChar++;
SendChar &= 0xFF;
}
Delay();Delay();Delay();Delay();
}
}
__interrupt void scicRxFifoIsr(void)
{
Uint16 i;
Recv_dat = ScicRegs.SCIRXBUF.all; // Read data
ScicRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
ScicRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x080; // Issue PIE ack
}
void scic_fifo_init()
{
ScicRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScicRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
// ScicRegs.SCICTL2.bit.TXINTENA =1;
ScicRegs.SCICTL2.bit.RXBKINTENA =1;
ScicRegs.SCIHBAUD = 0x01;
ScicRegs.SCILBAUD = 0xE7;//SCI_PRD;
ScicRegs.SCICCR.bit.LOOPBKENA =0; // Enable loop back
ScicRegs.SCIFFTX.all=0xC021;
ScicRegs.SCIFFRX.all=0x0021;
ScicRegs.SCIFFCT.all=0x00;
ScicRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
ScicRegs.SCIFFTX.bit.TXFIFOXRESET=1;
ScicRegs.SCIFFRX.bit.RXFIFORESET=1;
}
void InitScicGpio()
{
EALLOW;
GpioCtrlRegs.GPBPUD.bit.GPIO62 = 0; // Enable pull-up for GPIO62 (SCIRXDC)
GpioCtrlRegs.GPBPUD.bit.GPIO63 = 0; // Enable pull-up for GPIO63 (SCITXDC)
GpioCtrlRegs.GPBQSEL2.bit.GPIO62 = 3; // Asynch input GPIO62 (SCIRXDC)
GpioCtrlRegs.GPBMUX2.bit.GPIO62 = 1; // Configure GPIO62 for SCIRXDC operation
GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation
// GpioCtrlRegs.GPBDIR.bit.GPIO62 = 0; // Configure GPIO63 for SCITXDC operation
// GpioCtrlRegs.GPBDIR.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation
EDIS;
}
#endif
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#pragma CODE_SECTION(InitFlash, "ramfuncs");
#define CPU_FREQ 150E6
#define LSPCLK_FREQ CPU_FREQ/4
#define SCI_FREQ 100E3
#define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1
// Prototype statements for functions found within this file.
__interrupt void scibTxFifoIsr(void);
__interrupt void scibRxFifoIsr(void);
void scib_fifo_init(void);
Uint16 rdataB[8]; // Received data for SCI-A
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadEnd;
extern Uint16 RamfuncsRunStart;
extern Uint16 RamfuncsLoadSize;
void Delay()
{
unsigned int i,j;
for(i = 0;i < 500;i++)
for(j = 0;j < 500;j++);
}
unsigned char Recv_dat = 0x00;
void main(void)
{
Uint16 i;
unsigned char SendChar = 0x00;
InitSysCtrl();
InitSciGpio();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
InitFlash();
EALLOW;
PieVectTable.SCIRXINTB = &scibRxFifoIsr;
// PieVectTable.SCITXINTB = &scibTxFifoIsr;
EDIS;
scib_fifo_init(); // Init SCI-B
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER9.bit.INTx3=1; // PIE Group 9, INT3
// PieCtrlRegs.PIEIER9.bit.INTx4=1; // PIE Group 9, INT4
IER = 0x100;
EINT;
while(1)
{
ScibRegs.SCITXBUF=0xAA;
Delay();Delay();Delay();Delay();
Delay();Delay();Delay();Delay();
Delay();Delay();Delay();Delay();
SendChar++;
SendChar &= 0xFF;
}
}
/*
__interrupt void scibTxFifoIsr(void)
{
Uint16 i;
for(i=0; i< 8; i++)
{
ScibRegs.SCITXBUF=sdataB[i]; // Send data
}
for(i=0; i< 8; i++) //Increment send data for next cycle
{
sdataB[i] = (sdataB[i]-1) & 0x00FF;
}
ScibRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ACK
}
*/
__interrupt void scibRxFifoIsr(void)
{
Uint16 i;
unsigned char Recev_dat = 0x00;//Tried also for unsigned int
Recev_dat=ScibRegs.SCIRXBUF.all; // Read data
// ScibRegs.SCIFFRX.bit.RXFIFORESET = 1;
ScibRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
ScibRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
void scib_fifo_init()
{
ScibRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
// ScibRegs.SCICTL2.bit.TXINTENA =1;
ScibRegs.SCICTL2.bit.RXBKINTENA =1;
ScibRegs.SCIHBAUD = 0x01;
ScibRegs.SCILBAUD = 0xE7;//SCI_PRD;1e7
ScibRegs.SCICCR.bit.LOOPBKENA =0; // Enable loop back
ScibRegs.SCIFFTX.all=0xC021;
ScibRegs.SCIFFRX.all=0x0021;
ScibRegs.SCIFFCT.all=0x00;
ScibRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
ScibRegs.SCIFFTX.bit.TXFIFOXRESET=1;
ScibRegs.SCIFFRX.bit.RXFIFORESET=1;
}
#if 1
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#pragma CODE_SECTION(InitFlash, "ramfuncs");
#define CPU_FREQ 150E6
#define LSPCLK_FREQ CPU_FREQ/4
#define SCI_FREQ 100E3
#define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1
// Prototype statements for functions found within this file.
//__interrupt void scicTxFifoIsr(void);
__interrupt void scicRxFifoIsr(void);
void scic_fifo_init(void);
void InitScicGpio();
Uint16 rdataB[8]; // Received data for SCI-A
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadEnd;
extern Uint16 RamfuncsRunStart;
extern Uint16 RamfuncsLoadSize;
void Delay()
{
unsigned int i,j;
for(i = 0;i < 500;i++)
for(j = 0;j < 500;j++);
}
Uint16 Recv_dat = 0x00;
void main(void)
{
Uint16 i;
unsigned char SendChar = 0x00;
InitSysCtrl();
InitScicGpio();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
InitFlash();
EALLOW;
PieVectTable.SCIRXINTC = &scicRxFifoIsr;
// PieVectTable.SCITXINTB = &scibTxFifoIsr;
EDIS;
scic_fifo_init(); // Init SCI-B
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER8.bit.INTx5 = 1; // PIE Group 9, INT3
// PieCtrlRegs.PIEIER8.bit.INTx6=1; // PIE Group 9, INT4
IER |= 0x080;
EINT;
while(1)
{
for(i = 0;i < 8;i++)
{
ScicRegs.SCITXBUF=0x55;//SendChar;
Delay();Delay();Delay();Delay();
Delay();Delay();Delay();Delay();
// ScicRegs.SCICTL1.bit.RXENA = 1;
// Delay();Delay();Delay();Delay();
// while(ScicRegs.SCIFFTX.bit.TXFFST != 0);
SendChar++;
SendChar &= 0xFF;
}
Delay();Delay();Delay();Delay();
}
}
/*
__interrupt void scibTxFifoIsr(void)
{
Uint16 i;
for(i=0; i< 8; i++)
{
ScibRegs.SCITXBUF=sdataB[i]; // Send data
}
for(i=0; i< 8; i++) //Increment send data for next cycle
{
sdataB[i] = (sdataB[i]-1) & 0x00FF;
}
ScibRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ACK
}
*/
__interrupt void scicRxFifoIsr(void)
{
Uint16 i;
unsigned char dat = 0x0, dat1 = 0x0;
// dat = ScicRegs.SCIRXST.bit.RXRDY;
//Recv_dat = ScicRegs.SCIRXEMU; // Read data
Recv_dat = ScicRegs.SCIRXBUF.all; // Read data
// dat = ScicRegs.SCIRXST.all;
// dat1 = ScicRegs.SCIRXST.bit.RXRDY;
for(i=0;i<8;i++)
{
// rdataB[i] = ScicRegs.SCIRXBUF.all; // Read data
}
ScicRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
ScicRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x080; // Issue PIE ack
}
void scic_fifo_init()
{
ScicRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScicRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
// ScicRegs.SCICTL2.bit.TXINTENA =1;
ScicRegs.SCICTL2.bit.RXBKINTENA =1;
ScicRegs.SCIHBAUD = 0x01;
ScicRegs.SCILBAUD = 0xE7;//SCI_PRD;
ScicRegs.SCICCR.bit.LOOPBKENA =0; // Enable loop back
ScicRegs.SCIFFTX.all=0xC021;
ScicRegs.SCIFFRX.all=0x0021;
ScicRegs.SCIFFCT.all=0x00;
ScicRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
ScicRegs.SCIFFTX.bit.TXFIFOXRESET=1;
ScicRegs.SCIFFRX.bit.RXFIFORESET=1;
}
void InitScicGpio()
{
EALLOW;
GpioCtrlRegs.GPBPUD.bit.GPIO62 = 0; // Enable pull-up for GPIO62 (SCIRXDC)
GpioCtrlRegs.GPBPUD.bit.GPIO63 = 0; // Enable pull-up for GPIO63 (SCITXDC)
GpioCtrlRegs.GPBQSEL2.bit.GPIO62 = 3; // Asynch input GPIO62 (SCIRXDC)
GpioCtrlRegs.GPBMUX2.bit.GPIO62 = 1; // Configure GPIO62 for SCIRXDC operation
GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation
// GpioCtrlRegs.GPBDIR.bit.GPIO62 = 0; // Configure GPIO63 for SCITXDC operation
// GpioCtrlRegs.GPBDIR.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation
EDIS;
}
#endif
Thanks in Advance,
Narsimha.
#if 1#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#pragma CODE_SECTION(InitFlash, "ramfuncs");
#define CPU_FREQ 150E6#if 1#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#pragma CODE_SECTION(InitFlash, "ramfuncs");
#define CPU_FREQ 150E6#define LSPCLK_FREQ CPU_FREQ/4#define SCI_FREQ 100E3#define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1
// Prototype statements for functions found within this file.//__interrupt void scicTxFifoIsr(void);__interrupt void scicRxFifoIsr(void);void scic_fifo_init(void);void InitScicGpio();
Uint16 rdataB[8]; // Received data for SCI-A
extern Uint16 RamfuncsLoadStart;extern Uint16 RamfuncsLoadEnd;extern Uint16 RamfuncsRunStart;extern Uint16 RamfuncsLoadSize;
void Delay(){ unsigned int i,j; for(i = 0;i < 500;i++) for(j = 0;j < 500;j++);}
Uint16 Recv_dat = 0x00;void main(void){ Uint16 i; unsigned char SendChar = 0x00;
InitSysCtrl(); InitScicGpio(); DINT;
InitPieCtrl(); IER = 0x0000; IFR = 0x0000; InitPieVectTable();
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart); InitFlash();
EALLOW; PieVectTable.SCIRXINTC = &scicRxFifoIsr; EDIS;
scic_fifo_init(); // Init SCI-B
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block PieCtrlRegs.PIEIER8.bit.INTx5 = 1; // PIE Group 9, INT3 IER |= 0x080; EINT;
while(1) { for(i = 0;i < 8;i++) { ScicRegs.SCITXBUF=0xAA;//SendChar; Delay();Delay();Delay();Delay(); Delay();Delay();Delay();Delay();// Delay();Delay();Delay();Delay();// while(ScicRegs.SCIFFTX.bit.TXFFST != 0); SendChar++; SendChar &= 0xFF; } Delay();Delay();Delay();Delay(); }}
__interrupt void scicRxFifoIsr(void){
Recv_dat = ScicRegs.SCIRXBUF.all; // Read data
ScicRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag ScicRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag PieCtrlRegs.PIEACK.all|=0x080; // Issue PIE ack}
void scic_fifo_init(){ ScicRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback // No parity,8 char bits, // async mode, idle-line protocol ScicRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK, // Disable RX ERR, SLEEP, TXWAKE// ScicRegs.SCICTL2.bit.TXINTENA =1; ScicRegs.SCICTL2.bit.RXBKINTENA =1; ScicRegs.SCIHBAUD = 0x01; ScicRegs.SCILBAUD = 0xE7;//SCI_PRD; ScicRegs.SCICCR.bit.LOOPBKENA =0; // Enable loop back ScicRegs.SCIFFTX.all=0xC021; ScicRegs.SCIFFRX.all=0x0021; ScicRegs.SCIFFCT.all=0x00;
ScicRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset ScicRegs.SCIFFTX.bit.TXFIFOXRESET=1; ScicRegs.SCIFFRX.bit.RXFIFORESET=1;}
void InitScicGpio(){ EALLOW;
GpioCtrlRegs.GPBPUD.bit.GPIO62 = 0; // Enable pull-up for GPIO62 (SCIRXDC) GpioCtrlRegs.GPBPUD.bit.GPIO63 = 0; // Enable pull-up for GPIO63 (SCITXDC)
GpioCtrlRegs.GPBQSEL2.bit.GPIO62 = 3; // Asynch input GPIO62 (SCIRXDC)
GpioCtrlRegs.GPBMUX2.bit.GPIO62 = 1; // Configure GPIO62 for SCIRXDC operation GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation
// GpioCtrlRegs.GPBDIR.bit.GPIO62 = 0; // Configure GPIO63 for SCITXDC operation// GpioCtrlRegs.GPBDIR.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation EDIS;}#endif
#define LSPCLK_FREQ CPU_FREQ/4#define SCI_FREQ 100E3#define SCI_PRD (LSPCLK_FREQ/(SCI_FREQ*8))-1
// Prototype statements for functions found within this file.//__interrupt void scicTxFifoIsr(void);__interrupt void scicRxFifoIsr(void);void scic_fifo_init(void);void InitScicGpio();
Uint16 rdataB[8]; // Received data for SCI-A
extern Uint16 RamfuncsLoadStart;extern Uint16 RamfuncsLoadEnd;extern Uint16 RamfuncsRunStart;extern Uint16 RamfuncsLoadSize;
void Delay(){ unsigned int i,j; for(i = 0;i < 500;i++) for(j = 0;j < 500;j++);}
Uint16 Recv_dat = 0x00;void main(void){ Uint16 i; unsigned char SendChar = 0x00;
InitSysCtrl(); InitScicGpio(); DINT;
InitPieCtrl(); IER = 0x0000; IFR = 0x0000; InitPieVectTable();
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart); InitFlash();
EALLOW; PieVectTable.SCIRXINTC = &scicRxFifoIsr;// PieVectTable.SCITXINTB = &scibTxFifoIsr; EDIS;
scic_fifo_init(); // Init SCI-B
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block PieCtrlRegs.PIEIER8.bit.INTx5 = 1; // PIE Group 9, INT3// PieCtrlRegs.PIEIER8.bit.INTx6=1; // PIE Group 9, INT4 IER |= 0x080; EINT;
while(1) { for(i = 0;i < 8;i++) { ScicRegs.SCITXBUF=0x55;//SendChar; Delay();Delay();Delay();Delay(); Delay();Delay();Delay();Delay(); ScicRegs.SCICTL1.bit.RXENA = 1;// Delay();Delay();Delay();Delay();// while(ScicRegs.SCIFFTX.bit.TXFFST != 0); SendChar++; SendChar &= 0xFF; } Delay();Delay();Delay();Delay(); }}
__interrupt void scicRxFifoIsr(void){ Uint16 i;unsigned char dat = 0x0, dat1 = 0x0;
// dat = ScicRegs.SCIRXST.bit.RXRDY;//Recv_dat = ScicRegs.SCIRXEMU; // Read data
Recv_dat = ScicRegs.SCIRXBUF.all; // Read data// dat = ScicRegs.SCIRXST.all;// dat1 = ScicRegs.SCIRXST.bit.RXRDY; for(i=0;i<8;i++) {// rdataB[i] = ScicRegs.SCIRXBUF.all; // Read data }
ScicRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag ScicRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag PieCtrlRegs.PIEACK.all|=0x080; // Issue PIE ack}
void scic_fifo_init(){ ScicRegs.SCICCR.all =0x0005; // 1 stop bit, No loopback // No parity,8 char bits, // async mode, idle-line protocol ScicRegs.SCICTL1.all =0x0002; // enable TX, RX, internal SCICLK, // Disable RX ERR, SLEEP, TXWAKE// ScicRegs.SCICTL2.bit.TXINTENA =1; ScicRegs.SCICTL2.bit.RXBKINTENA =1; ScicRegs.SCIHBAUD = 0x01; ScicRegs.SCILBAUD = 0xE7;//SCI_PRD; ScicRegs.SCICCR.bit.LOOPBKENA =0; // Enable loop back ScicRegs.SCIFFTX.all=0xC021; ScicRegs.SCIFFRX.all=0x0021; ScicRegs.SCIFFCT.all=0x00;
ScicRegs.SCICTL1.all =0x0022; // Relinquish SCI from Reset ScicRegs.SCIFFTX.bit.TXFIFOXRESET=1; ScicRegs.SCIFFRX.bit.RXFIFORESET=1;}
void InitScicGpio(){ EALLOW;
GpioCtrlRegs.GPBPUD.bit.GPIO62 = 0; // Enable pull-up for GPIO62 (SCIRXDC) GpioCtrlRegs.GPBPUD.bit.GPIO63 = 0; // Enable pull-up for GPIO63 (SCITXDC)
GpioCtrlRegs.GPBQSEL2.bit.GPIO62 = 3; // Asynch input GPIO62 (SCIRXDC)
GpioCtrlRegs.GPBMUX2.bit.GPIO62 = 1; // Configure GPIO62 for SCIRXDC operation GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation
// GpioCtrlRegs.GPBDIR.bit.GPIO62 = 0; // Configure GPIO63 for SCITXDC operation// GpioCtrlRegs.GPBDIR.bit.GPIO63 = 1; // Configure GPIO63 for SCITXDC operation EDIS;}#endif