Part Number: LAUNCHXL-F28379D
Tool/software: Code Composer Studio
Hello
i am try to understaning the example of Trip_zone
what is the meaning of this loop and InputXbarRegs.INPUT1SELECT = 12; this one.
void InitTzGpio(void)
{
//
// For External Trigger, GPIO12 as the trigger for TripZone
//
GpioCtrlRegs.GPAPUD.bit.GPIO12 = 0; // Enable pull-up on GPIO12 (TZ1)
GpioCtrlRegs.GPAQSEL1.bit.GPIO12 = 3; // Asynch input GPIO12 (TZ1)
EALLOW;
InputXbarRegs.INPUT1SELECT = 12;
EDIS;
//
// For monitoring when the TZ Interrupt has been entered
//
EALLOW;
GpioCtrlRegs.GPAPUD.bit.GPIO11 = 1; // Disable pull-up on GPIO0 (EPWM1A)
GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 0; // Configure GPIO0 as EPWM1A
GpioCtrlRegs.GPADIR.bit.GPIO11 = 1;
EDIS;
}