Part Number: TMS320F28035
Tool/software: Code Composer Studio
Hi, I am having major problems getting my code to run from FLASH on a TMS320F28035.
My code (written in C) worked perfectly well when operating in DEBUG mode (in RAM) and the operation was as I expected. I have since attempted to create a version that I can program into FLASH which will boot and operate at power up.
I have followed the examples and methods described in the application note (SPRA958L) and also looked at a number of resolved enquiries in this forum -but no joy. I believe I have selected the correct example linker file (F28035.cmd as opposed to the 28035_RAM_Ink.cmd file). When I program the device, I get the dialogue indicating that FLASH is being erased and then written to and I can initiate the code using the green triangle or single step. However, when I power off and disconnect the XDS110, it will not start up. The XRS pin (reset) is pulsing low for ~50us every ~13ms, which suggests the watchdog is going off and resetting the device, yet I have (I believe) disabled it in the setup routine (ala SPRA958L).
I have included a cut down version of the code (I really do not want to bore any potential helpers with all the code) that just flashes a couple of LEDS. I am happy to post any extra data as necessary if someone can help.
I know it is going to be embarrassingly obvious – but at this point I would be happy for any help, as I have spent an awful of time trying to program the part.
J
Code below:
#include "DSP28x_Project.h"
#include "DSP2803x_Device.h"
//#include "DSP2803x_SysCtrl.c"
#include "DSP2803x_Adc.c"
#include "EP1401_DSP28035_GPIO.c"
//#include "DSP2803x_PieCtrl.c"
//#include "DSP2803x_PieVect.c
#include <string.h>
#include <stdint.h>
#pragma CODE_SECTION(InitFlash, "ramfuncs");
//Global Variables
int LEDToggleCount = 0; //Toggle count to allow the LED to be turned off and on.
int LED = 0; //LED state: 0 = ON, 1 = OFF.
void InitialisePorts(void)
{
EALLOW;
/*
* Set up functions of GPIO
*/
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3; //GPIO18 = XCKLOUT
//LED control bits
GpioCtrlRegs.GPAMUX2.bit.GPIO22 = 0b00; //GPIO
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 0b00; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 0b00; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 0b00; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 0b00; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 0b00; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 0b00; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 0b00; // GPIO functionality GPIO16-GPIO31
//Unused
GpioCtrlRegs.GPBMUX1.bit.GPIO42 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPBMUX1.bit.GPIO43 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 0; // GPIO functionality GPIO16-GPIO31
//COMMs data bits
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 0; // GPIO functionality GPIO16-GPIO31
//digital Data
GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPBMUX1.bit.GPIO44 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 0; // GPIO functionality GPIO16-GPIO31
GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; // GPIO functionality GPIO16-GPIO31
/*
* Set up direction of GPIO
*/
GpioCtrlRegs.GPADIR.bit.GPIO18 = 1; // GPIO are GP outputs XCLKOUT
//LEDS
GpioCtrlRegs.GPADIR.bit.GPIO22 = 1; // GPIO0-GPIO31 are GP outputs
GpioCtrlRegs.GPADIR.bit.GPIO29 = 1; // GPIO are GP outputs
GpioCtrlRegs.GPBDIR.bit.GPIO32 = 1; // GPIO are GP outputs
GpioCtrlRegs.GPBDIR.bit.GPIO33 = 1; // GPIO are GP outputs
GpioCtrlRegs.GPADIR.bit.GPIO9 = 1; // GPIO are GP outputs
GpioCtrlRegs.GPADIR.bit.GPIO28 = 1; // GPIO are GP outputs
GpioCtrlRegs.GPADIR.bit.GPIO23 = 1; // are GP outputs
GpioCtrlRegs.GPADIR.bit.GPIO26 = 1; // are GP outputs
//Spare
GpioCtrlRegs.GPBDIR.bit.GPIO42 = 1; // are GP outputs
GpioCtrlRegs.GPBDIR.bit.GPIO43 = 1; // are GP outputs
GpioCtrlRegs.GPADIR.bit.GPIO27 = 1; // are GP outputs
//COMMs data bits
GpioCtrlRegs.GPADIR.bit.GPIO0 = 0; // GPIO are GP input
GpioCtrlRegs.GPADIR.bit.GPIO1 = 1; // GPIO are GP output
GpioCtrlRegs.GPADIR.bit.GPIO2 = 1; // GPIO are GP output
GpioCtrlRegs.GPADIR.bit.GPIO3 = 1; // GPIO are GP input
GpioCtrlRegs.GPADIR.bit.GPIO4 = 0; // GPIO are GP input
GpioCtrlRegs.GPADIR.bit.GPIO5 = 1; // GPIO are GP output
GpioCtrlRegs.GPADIR.bit.GPIO6 = 1; // GPIO are GP output
GpioCtrlRegs.GPADIR.bit.GPIO7 = 0; // GPIO are GP input
//Digital data
GpioCtrlRegs.GPADIR.bit.GPIO8 = 0; // GPIO are GP input
GpioCtrlRegs.GPADIR.bit.GPIO25 = 0; // GPIO are GP input
GpioCtrlRegs.GPADIR.bit.GPIO2 = 0; // GPIO are GP input
GpioCtrlRegs.GPBDIR.bit.GPIO44 = 0; // GPIO are GP input
GpioCtrlRegs.GPBDIR.bit.GPIO41 = 0; // GPIO are GP input
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 0; // GPIO are GP input
//Disable interrupts
DINT;
//End edit of control registers
EDIS;
}
/*
*This section sets up the ADC to read the input voltages
*There are 5 inputs to read hence SOC0 to SOC4
*ADC operation is software driven and does NOT use any interrupts.
*A simple time delay is employed to provide time for the ADC operation
*/
void SetUpADC(void)
{
EALLOW;
//Single Sample Mode
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN0 = 0x00; //Single sample mode for 0 and 1
//ADC Port B-0 --TB_MEASURE_A Pin 23
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 0x00; //0x00 means Software triggers ADC process
AdcRegs.ADCSOC0CTL.bit.CHSEL = 0x08; //SOC0 = ADC-IP B0 Pin 23
AdcRegs.ADCSOC0CTL.bit.ACQPS = 0x09; //10 Clock Cycles Sample period
//ADC Port B-1 --MISSILE_P44V_A Pin 24
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 0x00; //0x00 means Software triggers ADC process
AdcRegs.ADCSOC1CTL.bit.CHSEL = 0x09; //SOC1 = ADC-IP B1 Pin 24
AdcRegs.ADCSOC1CTL.bit.ACQPS = 0x09; //10 Clock Cycles Sample period
//Single Sample Mode
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN2 = 0x00; //Single sample mode for 2 and 3
//ADC Port B-2 --28V_Sense_A Pin 25
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 0x00; //0x00 means Software triggers ADC process
AdcRegs.ADCSOC2CTL.bit.CHSEL = 0x0A; //SOC2 = ADC-IP B2 Pin 25
AdcRegs.ADCSOC2CTL.bit.ACQPS = 0x09; //10 Clock Cycles Sample period
//ADC Port B-3 --44V_Sense_A Pin 26
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 0x00; //0x00 means Software triggers ADC process
AdcRegs.ADCSOC3CTL.bit.CHSEL = 0x0B; //SOC3 = ADC-IP B3 Pin 26
AdcRegs.ADCSOC3CTL.bit.ACQPS = 0x09; //10 Clock Cycles Sample period
//Single Sample Mode
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN4 = 0x00; //Single sample mode for 4 and 5
//ADC Port B-4 --TB_GOOD Pin 27
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 0x00; //0x00 means Software triggers ADC process
AdcRegs.ADCSOC4CTL.bit.CHSEL = 0x0C; //SOC3 = ADC-IP B4 Pin 27
AdcRegs.ADCSOC4CTL.bit.ACQPS = 0x09; //10 Clock Cycles Sample period
EDIS;
}
/*
* This code intitilises the LEDS OFF
*/
void IntialiseLEDS(void)
{
GpioDataRegs.GPADAT.bit.GPIO22 = 0; //Turn on LED3 (RED)
GpioDataRegs.GPBDAT.bit.GPIO32 = 0; //Turn on LED4 (RED) ?
GpioDataRegs.GPBDAT.bit.GPIO33 = 0; //Turn on LED5 (RED)
GpioDataRegs.GPADAT.bit.GPIO23 = 0; //Turn on LED6 (RED)
GpioDataRegs.GPADAT.bit.GPIO29 = 0; //Turn on LED1 (GREEN) ?
GpioDataRegs.GPADAT.bit.GPIO26 = 0; //Turn on LED2 (GREEN)
GpioDataRegs.GPADAT.bit.GPIO9 = 0; //Turn on LED7 (GREEN)
GpioDataRegs.GPADAT.bit.GPIO28 = 0; //Turn on LED8 (GREEN)
GpioDataRegs.GPADAT.bit.GPIO22 = 1; //Turn off LED3 (RED)
GpioDataRegs.GPBDAT.bit.GPIO32 = 1; //Turn off LED4 (RED) ?
GpioDataRegs.GPBDAT.bit.GPIO33 = 1; //Turn off LED5 (RED)
GpioDataRegs.GPADAT.bit.GPIO23 = 1; //Turn off LED6 (RED)
GpioDataRegs.GPADAT.bit.GPIO29 = 1; //Turn off LED1 (GREEN) ?
GpioDataRegs.GPADAT.bit.GPIO26 = 1; //Turn off LED2 (GREEN)
GpioDataRegs.GPADAT.bit.GPIO9 = 1; //Turn off LED7 (GREEN)
GpioDataRegs.GPADAT.bit.GPIO28 = 1; //Turn off LED8 (GREEN)
}
/*
* This code initialises the communication control
*/
void InitialiseComms(void)
{
//GpioDataRegs.GPADAT.bit.GPIO1 = 0; //Allow WCU clock in
GpioDataRegs.GPADAT.bit.GPIO1 = 1; //TEST Disable WCU clock in
GpioCtrlRegs.GPAPUD.bit.GPIO0 = 1; //Disable the PU
GpioDataRegs.GPADAT.bit.GPIO2 = 1; //Allow Data out
GpioDataRegs.GPADAT.bit.GPIO5 = 0; //Allow RTL in
GpioDataRegs.GPADAT.bit.GPIO6 = 1; //Allow PMG Frequency out
}
/*
* This is the MAIN
*/
/*
* The following 'extern' statements have been added to overcome the flash issue.
*/
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadSize;
extern Uint16 RamfuncsRunStart;
//
extern Uint16 PieVectTableInit;
extern unsigned int econst_loadstart;
extern unsigned int econst_loadsize;
extern unsigned int econst_runstart;
void main(void)
{
memcpy(&RamfuncsRunStart,&RamfuncsLoadStart, (Uint32)&RamfuncsLoadSize);
InitSysCtrl();
InitGpio();
DINT;
//Following line added to attmept to fix the Flash issue (SPRA958L application note).
/*** Initialize the PIE_RAM ***/
// PieCtrlRegs.PIECTRL.bit.ENPIE = 0; // Disable the PIE
// EALLOW;
// memcpy((Uint16 *)&PieVectTable+6, (Uint16 *)&PieVectTableInit+6, 256-6);
InitAdc();
//Initialise the ports
InitialisePorts();
//Initialise the LEDS (off)
IntialiseLEDS();
//Enable the communications buffers
InitialiseComms();
//Configure the ADC
SetUpADC();
//read the PMG detected status
PMGConnected();
IntialiseLEDS(); //ODD - two of the LEDS are on when they should be off!!!!
GpioDataRegs.GPBDAT.bit.GPIO32 = 1;
GpioDataRegs.GPADAT.bit.GPIO29 = 1;
//test code
//end test code
while(1)
{
if (LEDToggleCount == 20)
{
GpioDataRegs.GPADAT.bit.GPIO22 = LED; //Toggle LED
LED = (!LED);
LEDToggleCount = 0;
}
else
{
LEDToggleCount++;
}
GpioDataRegs.GPADAT.bit.GPIO26 = 0; //Turn off LED2 (GREEN)
GpioDataRegs.GPADAT.bit.GPIO26 = 1; //Turn off LED2 (GREEN)
/*
* The sequnce will simply now repeat ad infinitum....
* or at least until the power is removed
*
*/
}
}