This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Dear TI Tech support,
Could you help me on this issue: Why I failed to program F28377S flash under CCS6.2
I created a F28377S binary (.out) code under CCS6.2.
1) under CCS6.2, using BH-USB560 v2 System Trace emulator, when I tried to program the DSP, I got the following error message (see below).
2) under CCS6.2, using XDS100v2 emulator, when I tried to program the DSP, I got the same error message (see below).
3) under uniFlash, using XDS100v2 emulator, the flash can be programmed successfully (see below).
Boot Selection pins on my control board were configured as wait mode: GPIO84 = 0 (pull_down 5k) ; GPIO72 = 1 (pull_up 10k) .
In CCS, the Target Configuration File was set accordingly when BH-USB560 v2 System Trace or XDS100v2 was used.
I also tried other emulators like BH-USB2000 and BH-USB510L, the issue remains same.
Thank you.
Keith
Under CCS6.2
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Error during Flash programming (Flash algorithm returned error code). Operation cancelled.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: C:\workspace\xwpro_porting_debug\PfrmB_XWP_6848-120_240-60\Base\Software\Code\SolarWave\Bin\ReleaseNoLoader\XWP.out: Load failed.
C28xx_CPU1: Error during Flash programming (Flash algorithm returned error code). Operation cancelled.
C28xx_CPU1: Please make sure the memory location you are programming have not already been programmed.
C28xx_CPU1: Error during Flash programming (Flash algorithm returned error code). Operation cancelled.
C28xx_CPU1: Please make sure the memory location you are programming have not already been programmed.
Under uniFlash
[5/18/2018, 9:32:50 AM] [INFO] C28xx_CPU1: GEL Output: Memory Map Initialization Complete
[5/18/2018, 9:35:28 AM] [SUCCESS] Program Load completed successfully.
[5/18/2018, 9:38:45 AM] [INFO] C28xx_CPU1: GEL Output: Memory Map Initialization Complete
[5/18/2018, 9:38:46 AM] [INFO] C28xx_CPU1: Erasing Flash memory...
[5/18/2018, 9:38:53 AM] [SUCCESS] C28xx_CPU1: Operation completed successfully.
[5/18/2018, 9:42:00 AM] [INFO] C28xx_CPU1: GEL Output: Memory Map Initialization Complete
[5/18/2018, 9:44:39 AM] [SUCCESS] Program Load completed successfully.
Hello Martin,
Thank you for your support.
I installed CCSv8 and I can open and compile/build my projects created under CCS6.2 now.
This is good.
Now I have one more question: since I have configured the Boot Selection pins on my control board to wait mode: GPIO84 = 0 (pull_down 5k) ; GPIO72 = 1 (pull_up 10k), have do I boot the code into flash at power up ?
Thank you.
Keith
Keith,
Please check Table 3-3. Device Default Boot Modes in Chapter 3 (ROM Code and Peripheral Booting) of the TRM.
Thanks and regards,
Vamsi
Hi Vamsi,
I set the Boot Config pins to the GetMode (IO84/72 = 1/1).
Now the DSP can boot to Flash with the emulator disconnected. I am happpy with this.
However, whenever I modify the firmware and try to program the flash again, I have to set the boot config pins back to the WaitMode (IO84/72 = 0/1).
My questions:
1) Is there a solution that will not require change the boot pins back and forth to support both the flash programming and power up to flash?
2) I used F28377D for long time. Why F28377D deos'nt needed the WaitMode to program the flash?
TI cliamed that D and S are compitable. That is why we changed the D to S to save the cost. Do you have any advices that will deal with the F28377S flash programing (our app requires upgrade firmware in field) ?
Thank you.
Keith
Keith
Regarding your question #1, if you plan on using JTAG, when you startup the device with JTAG connected and no emulation key is programmed, the device will go to wait boot.
Best regards
Chris
Hi Chris,
What do mean by "when you startup the device with JTAG connected" ?
You mean "turn on the power" or "start the CCS" ?
Thank you.
Keith
Hi Chris and TI tech supporters,
I think my platform (F28377S + CCSv8) is working OK now.
Thank you very much for the help.
Keith