Part Number: LAUNCHXL-F28379D
I've been using the LAUNCHXL-F28379D for over a year now, and there is one oddity that I haven't been able to figure out.
Regardless of the host OS, if I plug the LaunchXL into the computer and immediately try to communicate with it, it will never work. However, if, while connected, I press the reset button the LaunchXL, then data will work in both directions. I can see from the FTDI LEDs that data is being received from the computer, but I've verified that the F28379D cannot read it.
I've thought this could possibly be because I've set my baud rate to 921600 on SCI. However, whatever terminal or serial port software I use also sets the same baud rate when opening the port.
Is there something I'm missing? Is there a way to "reset" the FTDI chip from the host end?